Part Number: TMS320F28075
Tool/software: TI-RTOS
Hi,
I'm developing a project with SYS/BIOS. I'm currently using CCS 6.1.1 and compiler version TI v6.4.11.
I'm using
- SYS/BIOS 6.46.01.38;
- UIA 2.00.06.52;
- XDC tools 3.32.01.22.
Now I need to use compiler version TI v15.12.6.LTS. I've installed it on my PC and then I've selected it from the Property Windows.
Unfortunately when I compile my project I get the following error:
"Can't find the target named 'devkits.target.Generic' along the path 'C:/ti/bios_6_46_01_38/packages;C:/ti/uia_2_00_06_52/packages;C:/ti/ccsv6/ccs_base;C:/ti/xdctools_3_32_01_22_core/packages;..;': please check the spelling of the target's name and that it exists along this path. .xdchelp /Cp4pwm line 10 C/C++ Problem"
If I switch back to the previous compiler version v6.4.11 I get the same error: so I cannot compile my project any more, even if I use the old compiler version!
I get the same error with compiler version v6.4.12, too.
How can I fix this error?
Thank you.
Best Regards,
Demis