Other Parts Discussed in Thread: TMDSCNCD28035, TMDSCNCD28035ISO, CONTROLSUITE
Hi,
I am trying to test this solar DC-DC MPPT converter. But now I have problem with connecting it to GUI.
I read the DSP code. It seems all communication is done by GPIO 22 and GPIO 23.
But the only connection choice I have is the JTAG on the main board, which is also used for debugging. But it is connecting to GPIO 28 and 29.
GPIO 22 and 23 goes to H2 on the main board which is simply 10 pins there..
So which port am I suppose to use to connect it to GUI?
Thanks,
Dong