Hello
We currently working on a board to control a Brushless motor. Then we used the F28377s (Issued from the ControlCard and IDDK kit)
So we use CCS with the CMWare, we have some tool like the debugger Blackhawk.
For another need, I'm looking for the good Cpu:
We need to measure the Rms currrent consumed by a asynchrones tree-phase motor . (We can't know the motor angle position)
Then this motor is driven by a controller which make change the voltage and the frequency of the tree phase signal.
We must be plug between the controller and the motor to measure the current in the motor phase (I think we need measure only 2 phases..?)
The Idea is to measure the current via an ADC with a LEM into two phase and then deduce the Rms current.
Then by parametric search, I found the basic µC TMS320F28015.
But this device is not supported by the CMWare2000 :-(
So, my question is:
In your opinion, which smallest CPU could I use to measure the Rms current in an asynchrones tree-phase motor?
Is there some existing application notes? schematic? evaluation board? software? exemple?.....
Thank for your reply.