Dear all,
I have problem to make external mode with eZdsp TMS320F28335.
I use matlab 2016, I install ControlSuite+CSSV6 in the same directory TI.
I download the package C2000 from mathwork and I follow the example available in mathwork website for external mode, but every time I receive the same error.
SW1 of eZdsp TMS320F28335 is the manufacturer setting position.
I check the PIN of TX and RX and are the same from the matlab configuration and the datasheet.
Please note that exist USB (COM1) connection with the target for build but this connection is closed.
Thank you for your reply.
This is the error:
### Starting build procedure for model: test1
Code Generation 1
Elapsed: 23 sec
### Generating code into build folder: C:\Users\LENOVO\Desktop\test_eZdsp\TestM16_20decem\test1_ert_rtw
### Invoking Target Language Compiler on test1.rtw
### Using System Target File: C:\Program Files\MATLAB\R2016a\rtw\c\ert\ert.tlc
### Loading TLC function libraries
Warning: The data type "int8" uses a word size that is not available on the intended target.
Fixed-point signals using this data type will be put inside a larger word or multi words. When used,
extra software will be generated to force this larger word or multi words to emulate a smaller
word. This emulation is helpful when your prototype target and your final
production target are not the same. If the smaller word size does NOT exist
on the final production target, then consider increasing the word size to
one that is supported.
Warning: The data type "uint8" uses a word size that is not available on the intended target.
.
Warning: The data type "boolean" uses a word size that is not available on the intended target.
### Initial pass through model to cache user defined code
### Caching model source code
### Writing header file test1.h
### Writing header file test1_types.h
.
### Writing header file rtwtypes.h
### Writing header file multiword_types.h
### Writing source file test1.c
### Writing header file test1_private.h
### Writing source file test1_data.c
.
### Writing header file rtmodel.h
### Writing source file ert_main.c
### TLC code generation complete.
### Generating TLC interface API.
### Creating data type transition file test1_dt.h
### Evaluating PostCodeGenCommand specified in the model
### Using toolchain: Texas Instruments C2000 Code Generation Tools v6.0.0 | gmake (64-bit Windows)
### Creating 'C:\Users\LENOVO\Desktop\test_eZdsp\TestM16_20decem\test1_ert_rtw\test1.mk' ...
### Building 'test1': C:\PROGRA~1\MATLAB\R2016a\bin\win64\gmake -B -f test1.mk all
C:\Users\LENOVO\Desktop\test_eZdsp\TestM16_20decem\test1_ert_rtw>cd .
C:\Users\LENOVO\Desktop\test_eZdsp\TestM16_20decem\test1_ert_rtw>if "" == "" (C:\PROGRA~1\MATLAB\R2016a\bin\win64\gmake -B -f test1.mk all ) else (C:\PROGRA~1\MATLAB\R2016a\bin\win64\gmake -B -f test1.mk )
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="MW_c28xx_board.obj" "MW_c28xx_board.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="MW_c28xx_csl.obj" "MW_c28xx_csl.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="test1.obj" "test1.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="test1_data.obj" "test1_data.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="c2833xBoard_Realtime_Support.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/c2833xBoard_Realtime_Support.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="DSP2833x_MemCopy.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/DSP2833x_MemCopy.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="DSP2833x_CpuTimers.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/DSP2833x_CpuTimers.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="DSP2833x_DefaultIsr.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/DSP2833x_DefaultIsr.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="DSP2833x_GlobalVariableDefs.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/DSP2833x_GlobalVariableDefs.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="DSP2833x_PieCtrl.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/DSP2833x_PieCtrl.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="DSP2833x_PieVect.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/DSP2833x_PieVect.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="DSP2833x_SysCtrl.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/DSP2833x_SysCtrl.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 -s -v28 -ml --float_support=fpu32 --output_file="DSP2833x_usDelay.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/DSP2833x_usDelay.asm"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 -s -v28 -ml --float_support=fpu32 --output_file="DSP2833x_CodeStartBranch.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/DSP2833x_CodeStartBranch.asm"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 -s -v28 -ml --float_support=fpu32 --output_file="DSP2833x_ADC_cal.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/DSP2833x_ADC_cal.asm"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="DSP2833x_DMA.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/DSP2833x_DMA.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="c2833xSchedulerTimer0.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/c2833xSchedulerTimer0.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="ext_serial_pkt_c2000.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/ext_serial_pkt_c2000.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="datamodify.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/datamodify.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="rtiostream_serial_c28x_ext.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/rtiostream_serial_c28x_ext.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="ext_serial_utils_c2000.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/ext_serial_utils_c2000.c"
"C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/ext_serial_utils_c2000.c", line 383: warning: function "ExtSetPktWithACK" was declared but never referenced
"C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/ext_serial_utils_c2000.c", line 422: warning: function "ExtGetPkt" was declared but never referenced
"C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/ext_serial_utils_c2000.c", line 494: warning: function "ExtPktPending" was declared but never referenced
"C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/ext_serial_utils_c2000.c", line 587: warning: function "ExtOpenSerialConnection" was declared but never referenced
"C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/ext_serial_utils_c2000.c", line 635: warning: function "ExtCloseSerialConnection" was declared but never referenced
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="ext_svr_c2000.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/ext_svr_c2000.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="ext_svr_serial_transport_c2000.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/ext_svr_serial_transport_c2000.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="ext_work_c2000.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/ext_work_c2000.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="rtiostream_serial_interface_c2000.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/rtiostream_serial_interface_c2000.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="rtiostream_utils_c2000.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/rtiostream_utils_c2000.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="updown_c2000.obj" "C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/updown_c2000.c"
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/include" -v28 --float_support=fpu32 -ml --define="EXTMODE_DISABLEPRINTF" -v28 --float_support=fpu32 -ml -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DON_TARGET_WAIT_FOR_START=0 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DEXT_MODE=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DON_TARGET_WAIT_FOR_START=0 -DRT -DSTACK_SIZE=512 -DMODEL=test1 -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IC:/PROGRA~1/MATLAB/R2016a/simulink/include/sf_runtime -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem/test1_ert_rtw -IC:/Users/LENOVO/Desktop/test_eZdsp/TestM16_20decem -IC:/PROGRA~1/MATLAB/R2016a/extern/include -IC:/PROGRA~1/MATLAB/R2016a/simulink/include -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/R2016a/rtw/c/ert -IC:/PROGRA~1/MATLAB/R2016a/toolbox/coder/rtiostream/src/utils -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/R2016a/toolbox/shared/can/src/scanutil -IC:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/R2016a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/R2016a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="ert_main.obj" "ert_main.c"
"### Creating standalone executable "../test1.out" ..."
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/bin/cl2000 -z -IC:/ti/ccsv6/tools/compiler/C2000_~1.LTS/lib --stack_size=512 --warn_sections --heap_size=4096 --reread_libs --rom_model -m"test1.map" -l"rts2800_fpu32.lib" --define PWM_DMAACCESS=0 --define BOOT_FROM_FLASH=0 --output_file=../test1.out MW_c28xx_board.obj MW_c28xx_csl.obj test1.obj test1_data.obj c2833xBoard_Realtime_Support.obj DSP2833x_MemCopy.obj DSP2833x_CpuTimers.obj DSP2833x_DefaultIsr.obj DSP2833x_GlobalVariableDefs.obj DSP2833x_PieCtrl.obj DSP2833x_PieVect.obj DSP2833x_SysCtrl.obj DSP2833x_usDelay.obj DSP2833x_CodeStartBranch.obj DSP2833x_ADC_cal.obj DSP2833x_DMA.obj c2833xSchedulerTimer0.obj ext_serial_pkt_c2000.obj datamodify.obj rtiostream_serial_c28x_ext.obj ext_serial_utils_c2000.obj ext_svr_c2000.obj ext_svr_serial_transport_c2000.obj ext_work_c2000.obj rtiostream_serial_interface_c2000.obj rtiostream_utils_c2000.obj updown_c2000.obj ert_main.obj C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/src/c28335.cmd C:/Matlab/SupportPackages/R2016a/toolbox/target/supportpackages/tic2000/rtlib/IQmath_fpu32.lib C:/PROGRA~1/MATLAB/R2016a/toolbox/idelink/extensions/ticcs/c2000/c2833xPeripherals.cmd
<Linking>
"### Created: ../test1.out"
"### Successfully generated all binary outputs."
C:\Users\LENOVO\Desktop\test_eZdsp\TestM16_20decem\test1_ert_rtw>exit /B 0
"### Invoking postbuild tool "Download" ..."
C:/ti/ccsv6/tools/compiler/C2000_~1.LTS/../../../ccs_base/SCRIPT~1/bin/dss.bat C:\PROGRA~1\MATLAB\R2016a/toolbox/idelink/EXTENS~1/ticcs/ccsdemos/RUNPRO~1.JS C:\MATLAB\SUPPOR~1\R2016a\toolbox\target\SUPPOR~1\tic2000/CCS_CO~1/F28335~2.CCX ../test1.out
*** User inputs:
Target Configuration: C:\MATLAB\SUPPOR~1\R2016a\toolbox\target\SUPPOR~1\tic2000/CCS_CO~1/F28335~2.CCX
Program Name: ../test1.out
Board Name: unspecified (connect to first board)
CPU Name: unspecified (connect to first CPU)
*** Starting debug session...
*** Debug Session Name: Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator_0/C28xx
*** Board Name: Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator_0
*** CPU Name: C28xx
*** Connecting to target...
*** Loading the program to the target...
*** Program is running.
*** Disconnecting from target...
*** Terminating debug session...
*** LOAD & RUN DONE.
"### Done invoking postbuild tool."
### Successful completion of build procedure for model: test1
### Creating HTML report file test1_codegen_rpt.html
Build process completed successfully
Verbose mode is enabled for External mode. You can disable Verbose in Model Configuration Parameters > Hardware Implementation > Target Hardware Resources > External mode.
Failed to open serial port '\\.\COM1'. The reported error code is: 2 or 0x00000002. Possible causes are:
a) The target is not powered on.
b) The specified port number is not correct.
c) The specified bit rate is not supported by the host machine.
d) The previous connection was not closed correctly. If this is the case, you may need to re-start MATLAB.
action: EXT_CONNECT
Error occurred while executing External Mode MEX-file 'ext_serial_win32_comm':
Failed to connect to the target. Possible reasons for the failure:
a) The target is not switched on.
b) The target is not connected to your host machine.
c) The application for the model is not running on the target. You might have clicked the Stop button. If the Run button is not dimmed, click it. Otherwise, click the Build button, which downloads and runs your application on the target.
Caused by:
ExtOpenSerialConnection() returned an error. More details may be reported in the MATLAB command window.
Component: Simulink | Category: Model error
Unable to connect to the 'TI Delfino F2833x' target for 'test1'.
Component: Simulink | Category: Model error