This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

RTOS: Problem in procession of download . blind.out file

Genius 3800 points

Replies: 13

Views: 1716

Tool/software: TI-RTOS

HI

I am studying  RTOS of c2000

I have installed RTOS of c2000 in ccs 6.2 .  then I read the student study PDF:

IN "TI _RTOS_Kernnel_Workshop_student"  , I read follow :

 

then ,I do lab1 with my f28069 card . but ,  I meet problem.  :  when I download  that " blink.out" of 28xx ,    it can not be end of download .

like this:

 out file.path:

 

ccs show :

 

My f28069 card is fine ,  i tested it  whith download other .out.file .

I do now why TI support that blink.out can no download , plese support me.

thanks

best regard !

hunk.

 

  • Hi Yanzhen,

    Are you trying to load the F28069 with the Lab_01 solution .out file or the one you built?

    I have not used a F28069 controlSTICK recently, but the workshop docs say to use XDS100v1 not XDS100v2. Can you try the v1 instead?

    Todd
  • In reply to ToddMullanix:

    Yanzhen,

    I found a ControlStick and was able to connect (via a XDS100v1 target configuration) and download and run the solution blink_C28x.out file that was included in the solutions zip.

    Todd
  • In reply to ToddMullanix:

    Todd:
    I tried it as you said before , but it is fail . I use F28069M not F28069 , but i think that is not problem in "M" . I can download the .out file of other project ,such as motorware lab1 . . but can not download total of that blink_c28x.out . just part of it . my F28069M card is XDS100V2 , I tested and connect succesed. so I edit that soltions , replace that" V1".....
    before done above , I have changed the workspace's path as instruct PDF said , I use TI-RTOS ->workspace, as PDF said . do you think this is not problem ?

    I want to know , Is RTOS 'S lab1 different with normal project without RTOS. ? or what will do the nest step I should do ?
  • In reply to yanzhen fu:

    Are you trying to load the F28069M with the Lab_01 solution .out file or the one you built?

    Here is the solution one I successfully loaded

    blink_C28x.out

  • In reply to ToddMullanix:

    hi todd :

    I can download other project created .out file

    next:

    but when I change to RTOS workpace , download c280x blink.out :

    then;

    and end :

    If i click “ok”  then  click "run"  , it is seam program can run . but  led do not blink . .

    I donot  know which configration was wrong . 

    best regard

    hunk 

  • In reply to yanzhen fu:

    Hunk,

    Are you still having issues loading the .out file?

    -Ozino

  • In reply to Ozino Odharo:

    hi Ozino
    yes , I haven't resolved. please help
  • In reply to yanzhen fu:

    Hunk,

    Were you able to load the blink.out file Todd posted in his previous post?

    Regards,
    Ozino

    e2e.ti.com/.../blink_5F00_C28x.out

  • In reply to Ozino Odharo:

    hi Ozino
    NO , It still can not download !
  • In reply to yanzhen fu:

    Hi Hunk,

    I tried loading the .out file on different devices and was unable to replicate your issue. Are there anything specific settings you have configured on the board or in CCS? We don't own the source for the TI-RTOS Workshop but if you want to contact the group that own the source you can do so at: www.mindshareadvantage.com/

    I have talked to the Code Composer Studio team and they mentioned that a debug server log can be useful here. It is not generated by default. You would need to enable logging and then reproduce the issue. This wiki details the steps to enable the debug server logging feature.

    processors.wiki.ti.com/.../Troubleshooting_CCSv7

    Let me know if you have anymore questions.
     
    Regards,
    Ozino

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.