Part Number: TMS320F28055
Other Parts Discussed in Thread: MOTORWARE, C2000WARE
Tool/software: Code Composer Studio
Hi all,
We are developing a motor control system with 3 TMS320F28054Ms as controllers of 3 axes and a TMS320F28055 as control manager. Software tool is Code Composer Studio(Version: 6.1.2.00015) and control program based on motorware_1_01_00_17. All chips work at 60 MHz frequency. The communication between 3 TMS320F28054Ms and a TMS320F28055 uses SICs. All things are great right now.
We want to save some parameters into TMS320F28055's FLASH. So we tested flash programming with \TI\controlSUITE3.4.4\libs\utilities\flash_api\2805x\V100\example_ccsv5 project. The testing is all right.
But after I ported flash programming example into my TMS320F28055 control manager, I had troubles.
PIE Vector SARAM Locations used by the Boot ROM set as:
0x0D02 Flash_CPUScaleFactor 0xFF04 0x00BF(Decimal 12,582,660)
0x0D04 Flash_CallbackPtr NULL
After I run ' Flash_Erase((SECTORB),&FlashStatus) ' instruction by step over command my program stopped at 0x3FF67B (into Bootloader zone).
Who can help me to solve the problem. Thanks in advance.