Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Tool/software: TI C/C++ Compiler
Hi All,
Note: This is going to be a long post, so please hold back and relax before you read
I am posting this query in continuation to the problem posted here (e2e.ti.com/support/microcontrollers/c2000/f/171/t/654370), which I feel has went off track a bit. Also this could be useful to many others if not me.
I am explaining the issue from start (below) :
- I am working on a code where the main function calls another function 'lorlineshape()' in a loop, until a threshold condition is satisfied.
- The function 'lorlineshape()' , imports a set of arrays from a predefined '.c' file (HITRAN)
- This algorithm was working absolutely fine with smaller dataset. I had successfully run this algorithm with arrays (from HITRAN.c file) of size 31 each.
- With new requirement I need these HITRAN.c file's arrays to be of size 460 each. so the function 'lorlineshape()' imports a bigger data set, and then processes the data. I have to change a few constants as well for the calculations and with change in theory. but that doesnot change the functioning of the 'lorlineshape()' I have checked it explicitly.
- This is a test program where I have pulled this function out of the loop and just trying to see if the output is correct.
you will see ADC and DAC are initialized but they I expect them to not interfere with the functioning here.
// INCLUDING FILES #include "F28x_Project.h" // Device Headerfile and Examples Include File #include "math.h" interrupt void cpu_timer0_isr(void); void ConfigureDAC(void); void ConfigureADC(void); void SetupADCSoftware(void); void lorlineshape(); // function for lorentzian line shape calculation created by neetesh #define CPUFREQ_MHZ 200 float samplingFreq_hz = 10000; float samplingPeriod_us = 0; #define RESULTS_BUFFER_SIZE 1024 //buffer for storing conversion results (size must be multiple of 16) float Aquire[RESULTS_BUFFER_SIZE]; Uint16 AdcaResults[16]; Uint16 vmin = 10; Uint16 vmax = 3200; float dacOutput = 0; Uint16 resultsIndex = 0; Uint16 Index = 0; Uint16 c = 0; Uint16 d = 0; //************Lorentzian lineshape************************// float Temp = 25; // Temperature celcius float p = 1; // pressure in bar float X_C2H2 = 0.05; // concentration in % float L = 05; // path length in cm float simulated[912]; //simulted lorentzian //*********************************************************// float slp = 01; void main(void) { // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the F2837xD_SysCtrl.c file. InitSysCtrl(); // Step 2. Initialize GPIO: // This example function is found in the F2837xD_Gpio.c file and // illustrates how to set the GPIO to it's default state. InitGpio(); // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the F2837xD_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; InitPieVectTable(); //configureDAC(DAC_NUM); ConfigureDAC(); //Configure the ADCs and power them up ConfigureADC(); //Setup the ADCs for software conversions SetupADCSoftware(); // Map Cpu Timer0 interrupt function to the PIE vector table EALLOW; PieVectTable.TIMER0_INT = &cpu_timer0_isr; EDIS; // Initialize variables start here....................................................// for(resultsIndex = 0; resultsIndex < 1024; resultsIndex++) { Aquire[resultsIndex] = 0; } resultsIndex = 0; for(resultsIndex = 0; resultsIndex < 912; resultsIndex++) { simulated[resultsIndex] = 0; } resultsIndex = 0; //....................initialization of variable completed.......................................// samplingPeriod_us = (1000000.0/samplingFreq_hz); // Initialize Cpu Timers InitCpuTimers(); // Configure Cpu Timer0 to interrupt at specified sampling frequency ConfigCpuTimer(&CpuTimer0, CPUFREQ_MHZ, samplingPeriod_us); // SETTING TIMER REGISTERS AND ENABLING INTERRUPT FOR TIMER REGISTER // Start Cpu Timer0 CpuTimer0Regs.TCR.all = 0x4000; // Enable interrupt IER |= M_INT1; PieCtrlRegs.PIEIER1.bit.INTx7 = 1; EINT; ERTM; //testing the lineshape function lorlineshape(); // Infinite loop while(1) { } } // Writing ISR for timer 0 interrupt interrupt void cpu_timer0_isr(void) { // CpuTimer1Regs.TCR.all = 0x0000; // Start Cpu Timer1 to indicate begin of interrupt //convert, wait for completion,store results and start conversions immediately via software, ADCA AdcaRegs.ADCSOCFRC1.all = 0x0002; // SOC1 % Check the value while(AdcaRegs.ADCINTFLG.bit.ADCINT1 == 0);//wait for ADCA to complete, then acknowledge flag AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; AdcaResults[resultsIndex]= AdcaResultRegs.ADCRESULT1; //store results //Aquire[resultsIndex]= AdcaResultRegs.ADCRESULT1; //store results // AdcaResults = AdcaResultRegs.ADCRESULT1; if(resultsIndex<8) { resultsIndex++; //CpuTimer1Regs.TCR.all = 0x0030; // Reload Cpu Timer1 } else resultsIndex=0; DacaRegs.DACVALS.all = dacOutput; //dacoutput to pin ADCIN1/pin11 on board //slp = (((vmax*1.24121212)-(vmin*1.24121212))/1000); //slp = 2; if(Index<1000) { Index++; dacOutput = dacOutput + slp; } else { Index =0; dacOutput = vmin*(4096/3300); } PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge this interrupt to receive more interrupts from group 1 } void ConfigureDAC(void) { EALLOW; DacaRegs.DACCTL.bit.DACREFSEL = 1; // Use ADC references DacaRegs.DACCTL.bit.LOADMODE = 0; // Load on next SYSCLK DacaRegs.DACVALS.all = 0x0800; // Set mid-range DacaRegs.DACOUTEN.bit.DACOUTEN = 1; // Enable DAC EDIS; } void ConfigureADC(void) { EALLOW; //write configurations AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4 AdcaRegs.ADCCTL2.bit.RESOLUTION = 0; // set resolution 12 bit AdcaRegs.ADCCTL2.bit.SIGNALMODE =0; // set single Mode AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1; //Set pulse positions to late AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1; //power up the ADCs DELAY_US(1000); //delay for 1ms to allow ADC time to power up EDIS; } void SetupADCSoftware(void) { //ADCA //Select the channels to convert and end of conversion flag EALLOW; AdcaRegs.ADCSOC1CTL.bit.CHSEL = 5; //SOC1 will convert pin A0 AdcaRegs.ADCSOC1CTL.bit.ACQPS = 99; //sample window is acqps + 1 SYSCLK cycles AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1 flag AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared EDIS; } //lorentzian function simulation void lorlineshape(void) { //Declare required variables //HITRAN 2012 parameters v0,ST0,gamma_air,gamma_self,Ep extern float v0[460]; //wavenumber extern float ST0[460]; //line intensity extern float gamma_air[460]; //Air broadening coeff extern float gamma_self[460]; //self broadening coeff extern float Ep[460]; // lower state energy extern float n[460]; //temp. exponent (for lorentzian lineshape) extern float delta[460]; //pressure induce frequency shift (for lorentzian lineshape) float T = 27; float T0 = 296; float L = 05; float QT0 = 0; float QT = 0; float x_C2H2 = 0; float x_air = 0; //mole fraction of Air (1-mole fraction of C2H2) (for Lorentzian lineshape) float v = 0; //float a = 0; float c1 = 0; float c2 = 0; float c3 = 0; float c4 = 0; double c6 = 0; float ST = 0; float phi_lor = 0; float gamma_airj = 0; float gamma_selfj = 0; float v0_shift = 0; float delta_nu = 0; float phi_gauss = 0; double Doppler_nu = 0; float phi_voigt[900]; // voigt function float voigt_width = 0; // voigt width float d = 0; // Some more parameters from Yuvan Liue paper for voigt calculations float CL = 0; float CG = 0; float area = 0; float Tn = 0; #define A -0.83088E1 #define B 0.14484E1 #define C -0.25946E-2 #define D 0.84612E-5 //#define M 26.04; // molecular weight of C2H2 #define z 1.4388 // z = hc/k Uint16 i = 0; Uint16 j = 0; //==========================End of declarations===================================// for(i = 0; i < 900; i++) { phi_voigt[i] = 0; } T = T + 273; //Convert Celsius into Kelvin QT0 = A + (B*T0) + (C *(T0*T0)) + (D * (T0*T0*T0)); //partition sum QT = A + (B*T) + (C *(T*T)) + (D * (T*T*T)); c3 = (QT0/QT)*(T0/T); //p = 1; //pressure in bar x_C2H2 = X_C2H2/100; x_air = 1-x_C2H2; //Calculate voigt lineshape array for each individual linecenters while adding each //individual arrays in another array to get a complete profile for(j = 0; j<460; j++) { c1 = (float)(1-exp(-(double)(z*v0[j]/T))); c2 = (float)(1-exp(-(double)(z*v0[j]/T0))); c4 = (float)(pow((double)(T0/T),(double)n[j])); // c4 = (T0/T).^n c6 = (double)z*(double)Ep[j]*(double)((1/T)-(1/T0)); ST = ST0[j]*(c3*c1/c2)*exp(-c6); //=====================Lorentzian lineshape==============================// gamma_airj = gamma_air[j]*c4; gamma_selfj = gamma_self[j]*c4; delta_nu = 2*p*(gamma_airj*x_air + gamma_selfj*x_C2H2); //lorentzian Fwhm v0_shift = v0[j] + p*delta[j]; // line center shift , delta is shifting coeff //=====================Gaussian lineshape================================// Doppler_nu = (7.1623E-07)*sqrt((double)(T/44.01))*(double)v0[j]; // gaussian fwhm for(i = 0; i<900; i++) { v = 2314.556889 + 0.0015806722222222*i; //900 points //Dimensionless parameter from Yuvan Liue et al d = (delta_nu - Doppler_nu)/(delta_nu + Doppler_nu); //Weights for voigt calculations from Yuvan Liue et al CL = 11.59196 + 19.0083*d - 7.16976*d*d - 5.08992*d*d*d; CG = 5.5182 - 19.16575*d + 6.89559*d*d + 5.32796*d*d*d; //Voigt width from Olivero & Longbothum voigt_width = 0.5*(1.0692*delta_nu + sqrt(delta_nu*delta_nu*0.86639 + 4*Doppler_nu*Doppler_nu)); phi_lor = (voigt_width/6.28318531)/(((v-v0_shift)*(v-v0_shift)) + (voigt_width*voigt_width*0.25)); phi_gauss = (float)(((2/voigt_width)*0.469718639)*exp(-1*(((v-v0[j])/voigt_width)*((v-v0[j])/voigt_width)*2.77258872))); phi_voigt[i] = CL*phi_lor + CG*phi_gauss; area = area + 2*phi_voigt[i]; } Tn = (v-2314.556889)/1800; // b-a/n area = Tn*area; //Normalise individual lineshapes and add into an array for(i = 0; i<900; i++) { phi_voigt[i] = phi_voigt[i]/area; simulated[i] = simulated[i] + ST*p*x_C2H2*phi_voigt[i]*L; } area = 0; } for(i=0;i<900;i++) { simulated[i] = exp(-1*simulated[i]); } } //end of the program--------------------// // INCLUDING FILES #include "F28x_Project.h" // Device Headerfile and Examples Include File #include "math.h" interrupt void cpu_timer0_isr(void); void ConfigureDAC(void); void ConfigureADC(void); void SetupADCSoftware(void); void lorlineshape(); // function for lorentzian line shape calculation created by neetesh #define CPUFREQ_MHZ 200 float samplingFreq_hz = 10000; float samplingPeriod_us = 0; #define RESULTS_BUFFER_SIZE 1024 //buffer for storing conversion results (size must be multiple of 16) float Aquire[RESULTS_BUFFER_SIZE]; Uint16 AdcaResults[16]; Uint16 vmin = 10; Uint16 vmax = 3200; float dacOutput = 0; Uint16 resultsIndex = 0; Uint16 Index = 0; Uint16 c = 0; Uint16 d = 0; //************Lorentzian lineshape************************// float Temp = 25; // Temperature celcius float p = 1; // pressure in bar float X_C2H2 = 0.05; // concentration in % float L = 05; // path length in cm float simulated[912]; //simulted lorentzian //*********************************************************// float slp = 01; void main(void) { // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the F2837xD_SysCtrl.c file. InitSysCtrl(); // Step 2. Initialize GPIO: // This example function is found in the F2837xD_Gpio.c file and // illustrates how to set the GPIO to it's default state. InitGpio(); // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the F2837xD_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; InitPieVectTable(); //configureDAC(DAC_NUM); ConfigureDAC(); //Configure the ADCs and power them up ConfigureADC(); //Setup the ADCs for software conversions SetupADCSoftware(); // Map Cpu Timer0 interrupt function to the PIE vector table EALLOW; PieVectTable.TIMER0_INT = &cpu_timer0_isr; EDIS; // Initialize variables start here....................................................// for(resultsIndex = 0; resultsIndex < 1024; resultsIndex++) { Aquire[resultsIndex] = 0; } resultsIndex = 0; for(resultsIndex = 0; resultsIndex < 912; resultsIndex++) { simulated[resultsIndex] = 0; } resultsIndex = 0; //....................initialization of variable completed.......................................// samplingPeriod_us = (1000000.0/samplingFreq_hz); // Initialize Cpu Timers InitCpuTimers(); // Configure Cpu Timer0 to interrupt at specified sampling frequency ConfigCpuTimer(&CpuTimer0, CPUFREQ_MHZ, samplingPeriod_us); // SETTING TIMER REGISTERS AND ENABLING INTERRUPT FOR TIMER REGISTER // Start Cpu Timer0 CpuTimer0Regs.TCR.all = 0x4000; // Enable interrupt IER |= M_INT1; PieCtrlRegs.PIEIER1.bit.INTx7 = 1; EINT; ERTM; //testing the lineshape function lorlineshape(); // Infinite loop while(1) { } } // Writing ISR for timer 0 interrupt interrupt void cpu_timer0_isr(void) { // CpuTimer1Regs.TCR.all = 0x0000; // Start Cpu Timer1 to indicate begin of interrupt //convert, wait for completion,store results and start conversions immediately via software, ADCA AdcaRegs.ADCSOCFRC1.all = 0x0002; // SOC1 % Check the value while(AdcaRegs.ADCINTFLG.bit.ADCINT1 == 0);//wait for ADCA to complete, then acknowledge flag AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; AdcaResults[resultsIndex]= AdcaResultRegs.ADCRESULT1; //store results //Aquire[resultsIndex]= AdcaResultRegs.ADCRESULT1; //store results // AdcaResults = AdcaResultRegs.ADCRESULT1; if(resultsIndex<8) { resultsIndex++; //CpuTimer1Regs.TCR.all = 0x0030; // Reload Cpu Timer1 } else resultsIndex=0; DacaRegs.DACVALS.all = dacOutput; //dacoutput to pin ADCIN1/pin11 on board //slp = (((vmax*1.24121212)-(vmin*1.24121212))/1000); //slp = 2; if(Index<1000) { Index++; dacOutput = dacOutput + slp; } else { Index =0; dacOutput = vmin*(4096/3300); } PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge this interrupt to receive more interrupts from group 1 } void ConfigureDAC(void) { EALLOW; DacaRegs.DACCTL.bit.DACREFSEL = 1; // Use ADC references DacaRegs.DACCTL.bit.LOADMODE = 0; // Load on next SYSCLK DacaRegs.DACVALS.all = 0x0800; // Set mid-range DacaRegs.DACOUTEN.bit.DACOUTEN = 1; // Enable DAC EDIS; } void ConfigureADC(void) { EALLOW; //write configurations AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4 AdcaRegs.ADCCTL2.bit.RESOLUTION = 0; // set resolution 12 bit AdcaRegs.ADCCTL2.bit.SIGNALMODE =0; // set single Mode AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1; //Set pulse positions to late AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1; //power up the ADCs DELAY_US(1000); //delay for 1ms to allow ADC time to power up EDIS; } void SetupADCSoftware(void) { //ADCA //Select the channels to convert and end of conversion flag EALLOW; AdcaRegs.ADCSOC1CTL.bit.CHSEL = 5; //SOC1 will convert pin A0 AdcaRegs.ADCSOC1CTL.bit.ACQPS = 99; //sample window is acqps + 1 SYSCLK cycles AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1 flag AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared EDIS; } //lorentzian function simulation void lorlineshape(void) { //Declare required variables //HITRAN 2012 parameters v0,ST0,gamma_air,gamma_self,Ep extern float v0[460]; //wavenumber extern float ST0[460]; //line intensity extern float gamma_air[460]; //Air broadening coeff extern float gamma_self[460]; //self broadening coeff extern float Ep[460]; // lower state energy extern float n[460]; //temp. exponent (for lorentzian lineshape) extern float delta[460]; //pressure induce frequency shift (for lorentzian lineshape) float T = 27; float T0 = 296; float L = 05; float QT0 = 0; float QT = 0; float x_C2H2 = 0; float x_air = 0; //mole fraction of Air (1-mole fraction of C2H2) (for Lorentzian lineshape) float v = 0; //float a = 0; float c1 = 0; float c2 = 0; float c3 = 0; float c4 = 0; double c6 = 0; float ST = 0; float phi_lor = 0; float gamma_airj = 0; float gamma_selfj = 0; float v0_shift = 0; float delta_nu = 0; float phi_gauss = 0; double Doppler_nu = 0; float phi_voigt[900]; // voigt function float voigt_width = 0; // voigt width float d = 0; // Some more parameters from Yuvan Liue paper for voigt calculations float CL = 0; float CG = 0; float area = 0; float Tn = 0; #define A -0.83088E1 #define B 0.14484E1 #define C -0.25946E-2 #define D 0.84612E-5 //#define M 26.04; // molecular weight of C2H2 #define z 1.4388 // z = hc/k Uint16 i = 0; Uint16 j = 0; //==========================End of declarations===================================// for(i = 0; i < 900; i++) { phi_voigt[i] = 0; } T = T + 273; //Convert Celsius into Kelvin QT0 = A + (B*T0) + (C *(T0*T0)) + (D * (T0*T0*T0)); //partition sum QT = A + (B*T) + (C *(T*T)) + (D * (T*T*T)); c3 = (QT0/QT)*(T0/T); //p = 1; //pressure in bar x_C2H2 = X_C2H2/100; x_air = 1-x_C2H2; //Calculate voigt lineshape array for each individual linecenters while adding each //individual arrays in another array to get a complete profile for(j = 0; j<460; j++) { c1 = (float)(1-exp(-(double)(z*v0[j]/T))); c2 = (float)(1-exp(-(double)(z*v0[j]/T0))); c4 = (float)(pow((double)(T0/T),(double)n[j])); // c4 = (T0/T).^n c6 = (double)z*(double)Ep[j]*(double)((1/T)-(1/T0)); ST = ST0[j]*(c3*c1/c2)*exp(-c6); //=====================Lorentzian lineshape==============================// gamma_airj = gamma_air[j]*c4; gamma_selfj = gamma_self[j]*c4; delta_nu = 2*p*(gamma_airj*x_air + gamma_selfj*x_C2H2); //lorentzian Fwhm v0_shift = v0[j] + p*delta[j]; // line center shift , delta is shifting coeff //=====================Gaussian lineshape================================// Doppler_nu = (7.1623E-07)*sqrt((double)(T/44.01))*(double)v0[j]; // gaussian fwhm for(i = 0; i<900; i++) { v = 2314.556889 + 0.0015806722222222*i; //900 points //Dimensionless parameter from Yuvan Liue et al d = (delta_nu - Doppler_nu)/(delta_nu + Doppler_nu); //Weights for voigt calculations from Yuvan Liue et al CL = 11.59196 + 19.0083*d - 7.16976*d*d - 5.08992*d*d*d; CG = 5.5182 - 19.16575*d + 6.89559*d*d + 5.32796*d*d*d; //Voigt width from Olivero & Longbothum voigt_width = 0.5*(1.0692*delta_nu + sqrt(delta_nu*delta_nu*0.86639 + 4*Doppler_nu*Doppler_nu)); phi_lor = (voigt_width/6.28318531)/(((v-v0_shift)*(v-v0_shift)) + (voigt_width*voigt_width*0.25)); phi_gauss = (float)(((2/voigt_width)*0.469718639)*exp(-1*(((v-v0[j])/voigt_width)*((v-v0[j])/voigt_width)*2.77258872))); phi_voigt[i] = CL*phi_lor + CG*phi_gauss; area = area + 2*phi_voigt[i]; } Tn = (v-2314.556889)/1800; // b-a/n area = Tn*area; //Normalise individual lineshapes and add into an array for(i = 0; i<900; i++) { phi_voigt[i] = phi_voigt[i]/area; simulated[i] = simulated[i] + ST*p*x_C2H2*phi_voigt[i]*L; } area = 0; } for(i=0;i<900;i++) { simulated[i] = exp(-1*simulated[i]); } } //end of the program--------------------// - Here is the HITRAN.c file
/* HITRAN.c */ // table section declaration // #pragma DATA_SECTION(QuadratureTable,"QuadratureTableSection") // quadrature look-up table: contains 5 quadrants of sinusoid data points // HITRAN for C2H2 // line center (wavenumber cm-1) const float v0[460] = {2314.556889, 2314.565559, 2314.571374, 2314.571685, 2314.574408, 2314.578412, 2314.579849, 2314.584995, 2314.585739, 2314.586922, 2314.588594, 2314.589115, 2314.590525, 2314.592608, 2314.594641, 2314.59616, 2314.604137, 2314.609833, 2314.613928, 2314.613928, 2314.614655, 2314.61699, 2314.618404, 2314.618469, 2314.620158, 2314.625166, 2314.646848, 2314.648153, 2314.657735, 2314.658096, 2314.659406, 2314.66288, 2314.664363, 2314.666922, 2314.672655, 2314.672914, 2314.678129, 2314.681398, 2314.685223, 2314.688335, 2314.691075, 2314.692309, 2314.694834, 2314.694881, 2314.696534, 2314.698054, 2314.705101, 2314.706081, 2314.707129, 2314.715007, 2314.715147, 2314.715257, 2314.715257, 2314.715715, 2314.7357, 2314.736304, 2314.737647, 2314.739934, 2314.742541, 2314.744697, 2314.745142, 2314.746679, 2314.746729, 2314.75171, 2314.760747, 2314.765384, 2314.765417, 2314.767547, 2314.770241, 2314.779925, 2314.782861, 2314.784876, 2314.790934, 2314.791147, 2314.791504, 2314.80162, 2314.802525, 2314.802526, 2314.804833, 2314.807581, 2314.8103, 2314.811991, 2314.812231, 2314.813557, 2314.814962, 2314.816041, 2314.819989, 2314.81999, 2314.827323, 2314.830055, 2314.830078, 2314.830247, 2314.830295, 2314.832541, 2314.83535, 2314.839363, 2314.841044, 2314.850035, 2314.85111, 2314.851418, 2314.852246, 2314.856083, 2314.858131, 2314.861412, 2314.863164, 2314.864389, 2314.875386, 2314.876266, 2314.877752, 2314.884531, 2314.887954, 2314.888846, 2314.888861, 2314.893558, 2314.896936, 2314.897026, 2314.90589, 2314.906854, 2314.90997, 2314.913681, 2314.913841, 2314.913864, 2314.919183, 2314.923044, 2314.926842, 2314.926916, 2314.930712, 2314.930715, 2314.932407, 2314.939075, 2314.941759, 2314.941769, 2314.94469, 2314.949226, 2314.953279, 2314.954121, 2314.965254, 2314.970229, 2314.971931, 2314.973815, 2314.978475, 2314.984126, 2314.987948, 2314.988792, 2314.988798, 2314.992127, 2314.995938, 2314.998632, 2315.000127, 2315.001673, 2315.001932, 2315.00364, 2315.004366, 2315.005415, 2315.007149, 2315.009402, 2315.01405, 2315.023936, 2315.023973, 2315.029947, 2315.029949, 2315.037471, 2315.038357, 2315.042879, 2315.043597, 2315.046896, 2315.050983, 2315.055993, 2315.055993, 2315.06283, 2315.065221, 2315.065223, 2315.068542, 2315.069109, 2315.070163, 2315.070489, 2315.077334, 2315.077632, 2315.07881, 2315.078952, 2315.081992, 2315.084763, 2315.089688, 2315.094462, 2315.094616, 2315.094617, 2315.098339, 2315.0998, 2315.100065, 2315.104794, 2315.112849, 2315.116028, 2315.117167, 2315.118133, 2315.118133, 2315.120365, 2315.121992, 2315.134955, 2315.134955, 2315.13577, 2315.13577, 2315.138377, 2315.139604, 2315.144806, 2315.149886, 2315.149993, 2315.156452, 2315.161662, 2315.166284, 2315.167771, 2315.173412, 2315.177516, 2315.177517, 2315.179933, 2315.180547, 2315.185687, 2315.187331, 2315.188105, 2315.189057, 2315.191377, 2315.19356, 2315.1995, 2315.21013, 2315.211159, 2315.216318, 2315.218424, 2315.221269, 2315.227726, 2315.228335, 2315.230528, 2315.233773, 2315.234003, 2315.235834, 2315.241263, 2315.24394, 2315.243942, 2315.244687, 2315.245834, 2315.246886, 2315.24837, 2315.251081, 2315.251626, 2315.253508, 2315.256597, 2315.258996, 2315.259053, 2315.260026, 2315.260027, 2315.26269, 2315.265118, 2315.268415, 2315.271194, 2315.276736, 2315.281137, 2315.284979, 2315.289683, 2315.290341, 2315.29251, 2315.297229, 2315.301043, 2315.303496, 2315.305605, 2315.312207, 2315.316136, 2315.318633, 2315.321492, 2315.325734, 2315.327954, 2315.331884, 2315.333453, 2315.340786, 2315.343725, 2315.351038, 2315.351759, 2315.354305, 2315.361286, 2315.363147, 2315.366674, 2315.366772, 2315.369467, 2315.371537, 2315.37231, 2315.376416, 2315.376892, 2315.377088, 2315.377427, 2315.381934, 2315.3881, 2315.3898, 2315.393065, 2315.395168, 2315.396788, 2315.399305, 2315.40253, 2315.413617, 2315.417294, 2315.421988, 2315.422925, 2315.42425, 2315.426195, 2315.432665, 2315.435818, 2315.438088, 2315.438487, 2315.441196, 2315.441546, 2315.443577, 2315.448125, 2315.449538, 2315.453857, 2315.454295, 2315.454842, 2315.455305, 2315.458604, 2315.458604, 2315.474832, 2315.475132, 2315.480148, 2315.485399, 2315.485665, 2315.485946, 2315.486457, 2315.501383, 2315.503202, 2315.504812, 2315.52228, 2315.522585, 2315.523727, 2315.537418, 2315.543108, 2315.54733, 2315.549429, 2315.549525, 2315.5564, 2315.557683, 2315.559137, 2315.563117, 2315.570825, 2315.582945, 2315.583968, 2315.587777, 2315.587782, 2315.59181, 2315.59181, 2315.59681, 2315.600082, 2315.600803, 2315.602527, 2315.605769, 2315.606607, 2315.607833, 2315.614575, 2315.614868, 2315.630226, 2315.639227, 2315.639402, 2315.640633, 2315.64202, 2315.643915, 2315.64939, 2315.650544, 2315.650655, 2315.651431, 2315.65401, 2315.657849, 2315.662164, 2315.662166, 2315.665627, 2315.667623, 2315.670739, 2315.670987, 2315.67411, 2315.676684, 2315.67837, 2315.68213, 2315.682196, 2315.68376, 2315.690699, 2315.691565, 2315.699104, 2315.700591, 2315.702506, 2315.703771, 2315.704323, 2315.704614, 2315.704689, 2315.718393, 2315.719774, 2315.723342, 2315.730503, 2315.731951, 2315.735358, 2315.735358, 2315.737127, 2315.739481, 2315.741031, 2315.744131, 2315.747672, 2315.749426, 2315.752541, 2315.754642, 2315.760425, 2315.761125, 2315.763071, 2315.767471, 2315.768916, 2315.779533, 2315.781609, 2315.78192, 2315.78265, 2315.783708, 2315.789107, 2315.789258, 2315.796408, 2315.799055, 2315.799055, 2315.802446, 2315.802945, 2315.805331, 2315.80538, 2315.806559, 2315.807884, 2315.808024, 2315.81149, 2315.813503, 2315.820284, 2315.820783, 2315.824909, 2315.839384, 2315.841122, 2315.848558, 2315.849549, 2315.870594, 2315.874042, 2315.895728, 2315.898129, 2315.898228, 2315.89991, 2315.907643, 2315.909177, 2315.909578, 2315.909832, 2315.910499, 2315.918866, 2315.92079, 2315.922431, 2315.934561, 2315.942937, 2315.943149, 2315.949746, 2315.950001, 2315.95108, 2315.955764, 2315.95853, 2315.95862, 2315.962734, 2315.963882, 2315.964908, 2315.96809, 2315.972921}; // ST0 = line intensity*N, (N = 2.479E19) const float ST0[460] = {2.66E-08, 1.80E-08, 1.94E-10, 3.25E-10, 5.58E-06, 1.43E-01, 4.39E-08, 5.90E-09, 5.70E-11, 5.56E-06, 1.54E-10, 5.85E-09, 1.39E-07, 1.22E-10, 1.54E-10, 4.22E-09, 1.34E-04, 4.43E-05, 6.17E-06, 6.17E-06, 3.76E-06, 1.71E-10, 2.01E-06, 2.01E-06, 7.01E-08, 8.27E-05, 4.76E-09, 6.86E-09, 1.57E-10, 3.00E-08, 6.74E-09, 3.48E-10, 3.48E-10, 2.33E-06, 2.99E-08, 2.53E-06, 2.49E-10, 4.07E-10, 2.86E-04, 2.39E-06, 5.67E-07, 1.31E-06, 2.28E-06, 2.28E-06, 1.07E-07, 4.11E-10, 2.39E-06, 1.33E-10, 1.31E-06, 1.68E-02, 1.17E-03, 1.41E-10, 1.98E-10, 1.86E-10, 1.27E-10, 2.97E-05, 1.17E-03, 4.04E-07, 1.37E-06, 5.67E-05, 2.81E-05, 8.50E-04, 1.25E-07, 5.30E-08, 4.09E-10, 2.59E-06, 2.59E-06, 9.42E-11, 2.38E-06, 1.19E-04, 1.92E-10, 7.02E-09, 1.26E-10, 1.26E-10, 1.89E-10, 2.86E-06, 1.84E-06, 1.84E-06, 1.07E-04, 2.75E-09, 4.36E-06, 1.38E-05, 1.39E-10, 1.41E-10, 5.29E-06, 2.88E-10, 1.01E-08, 1.01E-08, 1.90E-08, 2.96E-06, 2.96E-06, 2.20E-10, 2.20E-10, 8.94E-10, 2.78E-10, 8.78E-08, 1.38E-05, 3.30E-09, 5.58E-10, 1.41E-08, 1.02E-04, 9.40E-08, 6.58E-10, 1.65E-04, 7.28E-05, 4.39E-09, 9.38E-08, 1.51E-10, 8.93E-07, 5.51E-10, 1.14E-09, 3.39E-06, 3.39E-06, 3.30E-04, 1.77E-10, 5.51E-10, 6.84E-07, 1.18E-08, 1.38E-09, 2.63E-10, 7.07E-08, 2.86E-10, 1.18E-08, 9.82E-10, 2.74E-06, 5.37E-08, 9.77E-09, 6.97E-09, 2.65E-10, 2.18E-07, 3.92E-06, 3.92E-06, 7.91E-11, 1.37E-09, 1.43E-04, 8.31E-09, 9.40E-05, 3.25E-10, 1.47E-06, 1.47E-04, 1.47E-06, 1.90E-08, 3.89E-10, 4.58E-06, 4.58E-06, 1.28E-10, 1.08E-07, 1.29E-10, 1.84E-08, 1.68E-04, 1.84E-08, 3.57E-10, 6.95E-08, 3.81E-06, 2.09E-10, 6.94E-08, 1.94E-06, 8.20E-06, 1.84E-08, 5.44E-06, 5.44E-06, 8.09E-10, 1.09E-05, 3.41E-06, 4.76E-05, 2.29E-10, 1.23E-04, 2.00E-08, 2.00E-08, 3.65E-11, 6.58E-06, 6.58E-06, 3.52E-10, 5.85E-10, 6.03E-09, 1.98E-04, 1.57E-08, 9.81E-07, 7.32E-08, 7.32E-08, 1.68E-10, 3.42E-10, 6.34E-08, 2.11E-10, 8.23E-06, 8.23E-06, 5.96E-08, 5.95E-08, 4.91E-10, 9.20E-02, 3.27E-09, 8.22E-07, 1.30E-10, 1.08E-05, 1.08E-05, 1.67E-04, 1.04E-10, 2.20E-04, 2.20E-04, 1.56E-05, 1.56E-05, 2.93E-05, 8.59E-07, 1.25E-05, 6.64E-06, 5.25E-06, 3.01E-04, 5.23E-06, 1.38E-10, 3.47E-06, 2.40E-04, 5.72E-06, 5.72E-06, 3.21E-06, 1.12E-10, 3.11E-10, 3.11E-10, 1.13E-10, 1.97E+01, 1.07E-01, 4.50E-10, 1.38E-07, 3.96E-04, 5.72E-04, 3.11E-08, 6.42E-09, 3.45E-03, 4.10E-08, 3.45E-03, 1.04E-03, 1.05E-10, 1.05E-10, 3.74E-10, 6.64E-08, 8.48E-09, 8.48E-09, 1.63E-10, 9.30E-08, 1.33E-07, 1.11E-07, 1.61E-10, 3.69E-10, 2.72E-11, 2.29E-10, 1.88E-10, 1.88E-10, 1.81E-10, 1.29E-10, 1.73E-10, 1.58E-08, 1.42E-06, 1.23E-10, 1.75E-10, 2.43E+00, 1.09E-10, 7.73E-10, 1.21E-08, 7.73E-08, 1.28E-06, 3.94E-06, 2.98E-08, 2.56E-09, 1.65E-04, 5.10E-04, 2.98E-08, 9.84E-07, 3.61E-09, 1.60E-03, 3.46E-10, 2.23E-10, 9.96E-09, 4.71E-08, 2.27E-10, 2.76E-10, 9.96E-09, 1.34E-06, 3.69E-02, 5.12E-09, 2.86E-04, 4.73E-10, 5.07E-09, 2.29E-10, 1.33E-06, 1.10E-09, 2.51E-06, 2.70E-10, 7.08E-11, 4.73E-10, 1.07E-10, 1.23E-09, 2.50E-06, 1.07E-10, 5.98E-07, 8.69E-08, 1.33E-05, 7.86E-07, 8.67E-08, 2.89E-08, 7.20E-06, 3.75E-06, 1.22E-09, 1.48E-01, 1.08E-09, 2.76E-06, 4.87E-09, 1.17E-04, 1.33E-05, 1.77E-10, 3.02E-10, 4.78E-09, 1.95E-07, 8.51E-11, 5.33E-09, 1.84E-06, 1.84E-06, 2.78E-10, 8.31E-06, 6.03E-08, 3.54E-05, 6.03E-08, 6.77E-08, 7.62E-09, 1.53E-03, 2.59E-10, 1.78E-10, 1.18E-06, 3.12E-08, 1.11E-10, 1.73E-08, 8.96E-11, 1.66E-08, 1.66E-08, 1.46E-10, 3.14E-08, 9.06E-11, 1.63E-08, 1.16E-03, 3.42E-06, 1.36E-08, 1.16E-03, 7.19E-09, 1.01E-08, 1.78E-08, 1.78E-08, 7.42E-10, 5.15E-11, 1.02E-07, 1.08E-06, 8.52E-07, 1.47E-10, 7.56E-07, 1.79E-10, 8.48E-08, 6.10E-10, 6.91E-08, 6.91E-08, 4.83E-10, 1.65E-06, 1.81E-02, 1.65E-06, 1.62E-04, 1.12E-10, 4.66E-10, 6.25E-06, 1.61E-04, 7.06E-09, 7.06E-09, 4.38E-06, 1.46E-08, 8.76E-11, 8.76E-11, 3.04E-09, 5.53E-08, 5.52E-08, 1.60E-10, 1.60E-10, 3.32E-10, 6.02E-08, 3.63E-10, 2.15E-09, 1.39E-10, 2.76E-10, 3.58E-06, 2.76E-10, 1.37E-10, 1.22E-05, 1.40E-06, 4.92E-06, 1.02E-08, 4.90E-06, 4.07E-10, 5.29E-06, 5.29E-06, 6.79E-08, 2.95E-09, 6.65E-10, 9.88E-08, 3.46E-11, 1.72E-10, 1.31E-08, 3.42E-07, 2.39E-10, 3.82E-09, 2.05E-10, 3.39E-10, 8.39E-09, 3.15E-06, 8.83E-11, 2.27E-10, 1.95E-10, 8.39E-09, 8.84E-11, 2.32E-10, 1.04E-05, 1.18E-10, 1.65E-10, 7.17E-10, 1.36E-07, 2.32E-04, 2.32E-04, 1.97E-10, 4.43E-05, 7.38E-06, 2.36E-08, 1.15E-10, 5.91E-10, 1.59E-10, 3.94E-10, 7.86E-07, 4.21E-08, 4.04E-10, 5.85E-09, 1.08E-09, 4.04E-10, 9.60E-09, 2.97E-10, 5.09E-06, 7.15E-11, 1.00E-08, 1.50E-10, 1.98E-10, 1.66E-06, 1.08E-09, 2.39E-05, 7.53E-09, 7.23E-11, 7.00E-08, 2.95E-08, 8.00E-08, 5.22E-08, 1.63E-10, 6.89E-07, 5.21E-08, 1.53E-01, 2.95E-08, 7.97E-08, 1.73E-07, 7.19E-11, 6.91E-11, 4.83E-10}; // ST0 = line intensity /*const float ST0[31] = { 5.89E-24, 5.06E-24, 5.36E-24, 8.37E-24, 1.61E-23, 1.97E-23, 2.79E-24, 2.17E-23, 9.92E-23, 2.00E-25, 7.21E-24, 3.17E-24, 1.21E-20, 2.49E-23, 2.10E-25, 8.79E-24, 1.52E-22, 5.06E-23, 3.97E-24, 1.58E-25, 9.39E-24, 1.77E-23, 1.43E-23, 1.50E-23, 4.99E-24, 6.62E-24, 5.99E-24, 2.82E-24, 8.47E-24, 7.78E-23, 1.98E-23 };*/ // Air broadening coeffcient const float gamma_air[460] = {0.0654, 0.0677, 0.0676, 0.0681, 0.0692, 0.0712, 0.0671, 0.0691, 0.0676, 0.0692, 0.0659, 0.0691, 0.0735, 0.0665, 0.0659, 0.0646, 0.0874, 0.0744, 0.0686, 0.0686, 0.0688, 0.0683, 0.0782, 0.0782, 0.062, 0.0794, 0.0652, 0.0675, 0.0626, 0.0747, 0.0675, 0.0679, 0.0679, 0.0677, 0.0747, 0.0614, 0.0664, 0.065, 0.0757, 0.0807, 0.0671, 0.0776, 0.0792, 0.0792, 0.0673, 0.0683, 0.0807, 0.0686, 0.0776, 0.0688, 0.0756, 0.0682, 0.0682, 0.0686, 0.0651, 0.0919, 0.0756, 0.068, 0.0693, 0.0763, 0.0878, 0.0878, 0.0677, 0.0681, 0.0648, 0.0803, 0.0803, 0.0677, 0.074, 0.0733, 0.0669, 0.0817, 0.0663, 0.0663, 0.0669, 0.0715, 0.0747, 0.0747, 0.0815, 0.0684, 0.0723, 0.0707, 0.0643, 0.0643, 0.0662, 0.0644, 0.066, 0.066, 0.0666, 0.0814, 0.0814, 0.0664, 0.0664, 0.067, 0.0684, 0.067, 0.0707, 0.0655, 0.0684, 0.0667, 0.0748, 0.0685, 0.0681, 0.0809, 0.0784, 0.0662, 0.0685, 0.0785, 0.0679, 0.0671, 0.0691, 0.0825, 0.0825, 0.0788, 0.0653, 0.0671, 0.0672, 0.0664, 0.0674, 0.0667, 0.0701, 0.0639, 0.0664, 0.0643, 0.0678, 0.0618, 0.0785, 0.0785, 0.0667, 0.0677, 0.0836, 0.0836, 0.0678, 0.0674, 0.0838, 0.0668, 0.0805, 0.0648, 0.0847, 0.0839, 0.0847, 0.0684, 0.0682, 0.0848, 0.0848, 0.0657, 0.0697, 0.0657, 0.0682, 0.0715, 0.0682, 0.065, 0.0671, 0.0682, 0.0628, 0.0671, 0.0612, 0.0688, 0.0679, 0.0858, 0.0858, 0.0685, 0.0882, 0.0805, 0.0815, 0.0686, 0.0827, 0.0679, 0.0679, 0.0675, 0.0868, 0.0868, 0.0695, 0.0705, 0.0654, 0.086, 0.0676, 0.0677, 0.0691, 0.0691, 0.0675, 0.0646, 0.07, 0.0663, 0.0877, 0.0877, 0.0686, 0.0686, 0.0695, 0.0778, 0.0798, 0.0673, 0.0679, 0.0886, 0.0886, 0.0849, 0.0658, 0.0805, 0.0805, 0.09, 0.09, 0.0869, 0.068, 0.0714, 0.0664, 0.069, 0.0879, 0.069, 0.0671, 0.0687, 0.087, 0.0685, 0.0685, 0.0679, 0.0641, 0.0678, 0.0678, 0.0641, 0.068, 0.0809, 0.0585, 0.0728, 0.0888, 0.0902, 0.071, 0.0849, 0.0859, 0.0615, 0.0859, 0.0955, 0.0662, 0.0662, 0.0682, 0.0874, 0.0659, 0.0659, 0.0668, 0.0874, 0.0621, 0.0676, 0.0668, 0.0687, 0.0668, 0.0642, 0.0663, 0.0663, 0.0681, 0.0681, 0.0685, 0.0665, 0.061, 0.0685, 0.0688, 0.0702, 0.068, 0.0669, 0.0666, 0.067, 0.0788, 0.074, 0.0738, 0.0653, 0.0867, 0.0892, 0.0738, 0.0674, 0.066, 0.0809, 0.0677, 0.0637, 0.0663, 0.068, 0.0666, 0.063, 0.0663, 0.0766, 0.0667, 0.0689, 0.0748, 0.067, 0.0689, 0.0666, 0.0766, 0.0668, 0.0797, 0.0748, 0.0677, 0.067, 0.0655, 0.0673, 0.0797, 0.0655, 0.0693, 0.0684, 0.0703, 0.0678, 0.0684, 0.0673, 0.0687, 0.068, 0.0673, 0.0717, 0.0689, 0.071, 0.0675, 0.0726, 0.0703, 0.0681, 0.0689, 0.0675, 0.0676, 0.0662, 0.0805, 0.0738, 0.0738, 0.0644, 0.0665, 0.067, 0.0871, 0.067, 0.0697, 0.0656, 0.0871, 0.0646, 0.0662, 0.0674, 0.0613, 0.0774, 0.0683, 0.0639, 0.0681, 0.0681, 0.0674, 0.0668, 0.0639, 0.0678, 0.0766, 0.0681, 0.0675, 0.0766, 0.0774, 0.0774, 0.0678, 0.0678, 0.0684, 0.0649, 0.0694, 0.0608, 0.0676, 0.0682, 0.068, 0.0639, 0.0671, 0.0682, 0.0689, 0.0689, 0.0691, 0.0837, 0.0689, 0.0837, 0.071, 0.065, 0.0692, 0.0729, 0.0828, 0.0657, 0.0657, 0.0681, 0.0666, 0.066, 0.066, 0.0642, 0.0685, 0.0685, 0.0662, 0.0662, 0.0692, 0.0697, 0.0632, 0.0651, 0.0667, 0.0677, 0.0795, 0.0677, 0.0667, 0.0709, 0.0675, 0.0688, 0.0664, 0.0688, 0.0681, 0.0684, 0.0684, 0.0668, 0.0658, 0.0668, 0.0675, 0.0639, 0.0635, 0.0663, 0.0678, 0.0683, 0.0788, 0.0644, 0.0681, 0.0662, 0.0685, 0.0653, 0.0646, 0.0665, 0.0662, 0.0653, 0.0642, 0.0667, 0.068, 0.068, 0.0682, 0.0721, 0.0795, 0.0795, 0.0665, 0.0826, 0.089, 0.0611, 0.0684, 0.0702, 0.0684, 0.0694, 0.0606, 0.068, 0.0669, 0.0666, 0.0673, 0.0669, 0.0657, 0.067, 0.0682, 0.0637, 0.0839, 0.066, 0.0684, 0.0676, 0.0673, 0.0876, 0.0645, 0.0637, 0.0925, 0.0731, 0.0682, 0.0669, 0.0675, 0.0678, 0.0669, 0.0778, 0.0731, 0.0682, 0.0675, 0.0645, 0.0655, 0.0698}; //self broadening coeff. const float gamma_self[460] = {0.069, 0.079, 0.078, 0.085, 0.093, 0.097, 0.074, 0.092, 0.081, 0.093, 0.07, 0.092, 0.1, 0.071, 0.07, 0.068, 0.117, 0.102, 0.09, 0.09, 0.09, 0.088, 0.105, 0.105, 0.065, 0.106, 0.069, 0.08, 0.066, 0.102, 0.08, 0.083, 0.083, 0.082, 0.102, 0.065, 0.072, 0.068, 0.103, 0.108, 0.076, 0.104, 0.106, 0.106, 0.079, 0.087, 0.108, 0.09, 0.104, 0.091, 0.103, 0.087, 0.087, 0.09, 0.069, 0.124, 0.103, 0.087, 0.093, 0.103, 0.118, 0.118, 0.082, 0.084, 0.068, 0.107, 0.107, 0.082, 0.101, 0.1, 0.074, 0.109, 0.071, 0.071, 0.074, 0.098, 0.102, 0.102, 0.109, 0.088, 0.099, 0.097, 0.067, 0.067, 0.071, 0.067, 0.071, 0.071, 0.072, 0.108, 0.108, 0.072, 0.072, 0.075, 0.089, 0.077, 0.097, 0.069, 0.088, 0.073, 0.102, 0.089, 0.087, 0.108, 0.105, 0.071, 0.089, 0.105, 0.081, 0.075, 0.093, 0.11, 0.11, 0.106, 0.069, 0.075, 0.076, 0.072, 0.08, 0.074, 0.096, 0.067, 0.072, 0.067, 0.083, 0.065, 0.105, 0.105, 0.074, 0.082, 0.111, 0.111, 0.083, 0.08, 0.112, 0.073, 0.108, 0.068, 0.113, 0.111, 0.113, 0.088, 0.087, 0.113, 0.113, 0.07, 0.094, 0.07, 0.086, 0.098, 0.086, 0.068, 0.076, 0.085, 0.066, 0.076, 0.064, 0.09, 0.081, 0.114, 0.114, 0.089, 0.118, 0.107, 0.108, 0.09, 0.11, 0.083, 0.083, 0.079, 0.116, 0.116, 0.094, 0.096, 0.069, 0.115, 0.078, 0.079, 0.093, 0.093, 0.077, 0.068, 0.095, 0.072, 0.117, 0.117, 0.09, 0.09, 0.094, 0.105, 0.107, 0.077, 0.084, 0.119, 0.119, 0.113, 0.07, 0.107, 0.107, 0.121, 0.121, 0.116, 0.083, 0.098, 0.071, 0.092, 0.118, 0.092, 0.075, 0.089, 0.116, 0.089, 0.089, 0.084, 0.067, 0.082, 0.082, 0.067, 0.083, 0.108, 0.063, 0.1, 0.119, 0.121, 0.097, 0.113, 0.114, 0.065, 0.114, 0.13, 0.071, 0.071, 0.086, 0.117, 0.07, 0.07, 0.073, 0.117, 0.065, 0.081, 0.073, 0.091, 0.073, 0.067, 0.072, 0.072, 0.086, 0.086, 0.089, 0.071, 0.064, 0.089, 0.09, 0.095, 0.085, 0.074, 0.073, 0.076, 0.106, 0.101, 0.101, 0.069, 0.116, 0.12, 0.101, 0.078, 0.07, 0.108, 0.082, 0.067, 0.072, 0.083, 0.074, 0.066, 0.072, 0.103, 0.073, 0.092, 0.102, 0.075, 0.092, 0.074, 0.103, 0.075, 0.107, 0.102, 0.079, 0.075, 0.069, 0.079, 0.107, 0.069, 0.093, 0.088, 0.096, 0.08, 0.088, 0.076, 0.089, 0.085, 0.079, 0.098, 0.092, 0.097, 0.079, 0.1, 0.096, 0.086, 0.092, 0.079, 0.081, 0.071, 0.107, 0.101, 0.101, 0.067, 0.072, 0.075, 0.116, 0.075, 0.095, 0.069, 0.116, 0.068, 0.071, 0.079, 0.064, 0.104, 0.087, 0.067, 0.085, 0.085, 0.076, 0.073, 0.067, 0.08, 0.103, 0.084, 0.077, 0.103, 0.104, 0.104, 0.082, 0.082, 0.088, 0.068, 0.093, 0.064, 0.078, 0.087, 0.082, 0.067, 0.078, 0.087, 0.092, 0.092, 0.093, 0.111, 0.092, 0.111, 0.097, 0.068, 0.093, 0.1, 0.11, 0.07, 0.07, 0.086, 0.072, 0.07, 0.07, 0.067, 0.089, 0.089, 0.071, 0.071, 0.093, 0.094, 0.066, 0.068, 0.073, 0.081, 0.106, 0.081, 0.073, 0.097, 0.079, 0.091, 0.072, 0.091, 0.086, 0.088, 0.088, 0.075, 0.07, 0.074, 0.08, 0.067, 0.066, 0.071, 0.085, 0.088, 0.106, 0.067, 0.085, 0.071, 0.088, 0.069, 0.068, 0.073, 0.071, 0.069, 0.067, 0.072, 0.085, 0.085, 0.088, 0.099, 0.106, 0.106, 0.073, 0.11, 0.12, 0.064, 0.088, 0.095, 0.088, 0.094, 0.064, 0.082, 0.074, 0.072, 0.078, 0.074, 0.07, 0.074, 0.087, 0.066, 0.111, 0.071, 0.089, 0.08, 0.078, 0.117, 0.067, 0.066, 0.125, 0.1, 0.087, 0.074, 0.077, 0.079, 0.074, 0.105, 0.1, 0.087, 0.08, 0.068, 0.069, 0.095}; //lower state energy const float Ep[460] = {3313.8391, 5017.6738, 6042.7964, 3163.8845, 2308.0605, 186.271, 4712.9653, 2853.9365, 1235.2485, 2308.6814, 4760.8252, 2853.9321, 1353.7441, 6082.9966, 4760.7988, 3009.3945, 1263.8425, 2052.0242, 2310.3225, 2310.3225, 3703.0286, 1050.7097, 1399.0031, 1399.0031, 2154.1006, 1993.5701, 2052.4016, 3155.2571, 2708.5469, 3094.5859, 3155.2483, 4174.9229, 4174.9209, 1209.1936, 3094.7397, 3054.1663, 4643.9229, 5724.4189, 2679.0798, 1958.3853, 1458.7273, 2131.062, 1389.1235, 1389.1235, 1916.5863, 4114.8125, 1958.4802, 2367.8911, 2131.2263, 352.002, 767.9741, 2377.1753, 2377.1753, 2368.6584, 3204.6477, 0, 767.8159, 1596.1239, 2227.7881, 2026.2404, 3008.6704, 2007.9543, 3159.0044, 4763.9683, 3139.5828, 1380.0038, 1380.0038, 1206.6031, 3833.2124, 2894.6177, 4198.2803, 1398.0176, 4308.5337, 4308.5352, 4200.8223, 3838.7932, 2098.8792, 2098.8792, 1975.5542, 1678.4587, 154.2009, 2088.1738, 4662.728, 4658.3726, 2540.1562, 5805.1255, 3752.3252, 3752.3252, 4902.2861, 1371.6439, 1371.6439, 2894.8474, 2894.8469, 4360.2939, 1027.1632, 1973.3499, 2088.5742, 5288.9053, 2415.8596, 3660.8093, 2903.3738, 3322.137, 1658.2191, 2713.9932, 2003.5808, 5212.2046, 3322.636, 2387.4214, 4053.7383, 3975.4548, 2570.9744, 1364.0439, 1364.0439, 2609.3755, 5335.9771, 3972.9099, 1424.8629, 3707.8088, 2470.1768, 2843.9382, 1552.9131, 5803.7959, 3707.6733, 3009.0676, 1181.1644, 2211.4319, 1382.0248, 1382.0247, 2841.9929, 3046.52, 1357.2039, 1357.2039, 1178.691, 2471.3535, 1960.6711, 5057.0952, 1984.0459, 5774.3467, 674.7094, 1386.4797, 674.7313, 3175.9939, 2438.5559, 1351.1237, 1351.1237, 4801.8105, 2770.6604, 4801.7817, 3195.4641, 2853.2878, 3195.4407, 5751.2295, 3313.9832, 3735.1338, 2653.4062, 3313.9961, 3111.7419, 3546.1982, 4995.9834, 1345.8035, 1345.8035, 3963.927, 1380.5728, 2372.2922, 39.2611, 1004.3515, 1967.636, 3197.1816, 3197.1816, 1939.5654, 1341.2433, 1341.2433, 2139.0908, 4038.5361, 2006.9584, 1948.9209, 5051.1162, 4051.2175, 1571.2661, 1571.2642, 6077.7368, 3179.4199, 2868.0254, 4681.8857, 1337.4432, 1337.4432, 2920.0449, 2920.0515, 2139.6013, 1470.1188, 3390.8381, 1391.7325, 1151.512, 1334.403, 1334.403, 1954.3514, 6135.0391, 1365.7964, 1365.7965, 1332.1228, 1332.1228, 1283.6475, 4049.3247, 803.3533, 2497.1599, 2327.9578, 1940.304, 2328.6265, 2735.5176, 3726.1357, 1944.1924, 2332.5234, 2332.5234, 1153.8716, 4710.623, 4203.5532, 4203.5508, 4706.1372, 578.0116, 1386.8291, 4072.0149, 1366.5837, 1937.1591, 1934.8203, 4867.6289, 1273.6547, 677.8777, 2269.512, 677.8545, 1933.2517, 4349.5825, 4349.584, 4140.3467, 669.429, 3793.0403, 3793.0403, 4235.3135, 669.4181, 2952.3447, 3187.6626, 4237.9614, 982.2749, 2298.0486, 5856.8232, 2931.396, 2931.3953, 2401.5278, 2401.5276, 2389.938, 4943.5303, 3178.0359, 2390.7583, 3629.9919, 921.2381, 1125.0663, 4394.5762, 3697.6707, 2003.9279, 2646.1621, 3731.4021, 3107.3701, 5335.9771, 1266.7874, 2077.6367, 3107.5432, 1359.3367, 5255.8848, 2400.2432, 1901.3584, 5857.2573, 3746.1907, 4793.9155, 2878.2937, 2599.014, 3746.0437, 2141.6709, 994.2385, 2875.2158, 2691.6206, 4011.1475, 2875.2107, 2876.2649, 2141.8606, 3025.8643, 1966.7233, 3458.6938, 4051.2175, 4008.4941, 4843.5244, 2499.4321, 1966.8372, 4843.4932, 3476.9836, 3344.7979, 2105.1194, 4085.0811, 3345.3303, 4784.0522, 3569.1978, 1127.3151, 2500.667, 170.0759, 2590.0884, 3855.887, 3185.532, 2909.4944, 2105.5562, 1099.3541, 960.9333, 3185.5227, 3075.2249, 6167.0889, 1405.3678, 2111.821, 2111.821, 3224.8882, 2454.9517, 3347.9385, 3011.7639, 3347.9524, 1570.0634, 1962.269, 2011.0934, 5823.5435, 4720.5762, 1327.6753, 2328.3401, 2396.8921, 3201.0125, 4759.2495, 3222.0454, 3222.019, 6111.1514, 4790.3345, 4754.6318, 5025.5737, 755.8286, 3763.3772, 5085.334, 755.6889, 1391.6066, 1391.6064, 3226.1389, 3226.1389, 3987.9595, 5432.46, 2790.3672, 3236.9551, 4085.0361, 1074.3752, 4080.9568, 5909.3003, 1974.2026, 2439.4937, 1590.6039, 1590.6016, 940.3268, 679.7121, 329.2988, 679.7413, 2870.5774, 3248.7566, 2158.1929, 139.5169, 1392.3757, 3834.4922, 3834.4922, 1101.4951, 2341.9949, 4391.3877, 4391.3896, 3111.3684, 2943.6003, 2943.6077, 2968.6582, 2968.6575, 2158.7439, 2886.9202, 2545.375, 5383.8286, 4273.1001, 4232.9351, 2380.3279, 4232.9326, 4275.856, 817.7256, 1296.7484, 2348.5911, 3735.2673, 2349.3096, 2462.8691, 2355.4634, 2355.4634, 2035.2397, 5300.4668, 4429.585, 3217.0542, 3841.1904, 5911.499, 4986.0791, 1642.5229, 1050.1302, 3400.3757, 5875.125, 4166.6309, 3785.3081, 3752.282, 4885.9668, 5850.397, 2913.3633, 3785.1492, 4885.9331, 3265.9456, 2413.5137, 2426.6169, 2426.6169, 1633.916, 1380.1362, 1373.9261, 1373.9261, 2911.2493, 32.1229, 1378.3, 2387.9163, 2412.7188, 4057.3723, 2413.5942, 920.4556, 3304.9934, 4822.0732, 4047.5962, 5137.2446, 2529.3992, 4044.8328, 1918.3337, 3544.365, 1076.4117, 4808.6069, 1278.7942, 4759.9946, 1026.6187, 1266.5563, 2530.6938, 1279.8604, 3559.2041, 4803.856, 2340.0134, 3120.906, 3368.189, 3382.6296, 4119.6392, 4117.2041, 3382.6443, 1367.4026, 3121.0994, 3368.7556, 3104.6641, 3683.96, 6225.5908, 3035.5212}; //Temperature coeff. const float n[460] = {0.69, 0.75, 0.75, 0.76, 0.74, 0.72, 0.73, 0.74, 0.75, 0.74, 0.71, 0.74, 0.69, 0.72, 0.71, 0.68, 0.77, 0.69, 0.75, 0.75, 0.75, 0.76, 0.69, 0.69, 0.66, 0.69, 0.69, 0.75, 0.66, 0.69, 0.75, 0.76, 0.76, 0.76, 0.69, 0.65, 0.72, 0.69, 0.69, 0.7, 0.74, 0.69, 0.69, 0.69, 0.75, 0.76, 0.7, 0.75, 0.69, 0.75, 0.69, 0.76, 0.76, 0.75, 0.69, 0.78, 0.69, 0.76, 0.74, 0.69, 0.77, 0.77, 0.76, 0.76, 0.69, 0.69, 0.69, 0.76, 0.69, 0.7, 0.73, 0.7, 0.72, 0.72, 0.73, 0.71, 0.69, 0.69, 0.7, 0.76, 0.7, 0.72, 0.68, 0.68, 0.71, 0.68, 0.71, 0.71, 0.72, 0.7, 0.7, 0.73, 0.73, 0.74, 0.75, 0.75, 0.72, 0.7, 0.76, 0.73, 0.69, 0.75, 0.76, 0.7, 0.69, 0.71, 0.75, 0.69, 0.75, 0.74, 0.74, 0.71, 0.71, 0.69, 0.69, 0.74, 0.74, 0.72, 0.75, 0.74, 0.73, 0.67, 0.72, 0.68, 0.76, 0.65, 0.69, 0.69, 0.74, 0.76, 0.72, 0.72, 0.76, 0.75, 0.72, 0.73, 0.69, 0.68, 0.74, 0.73, 0.74, 0.76, 0.76, 0.73, 0.73, 0.71, 0.73, 0.71, 0.76, 0.71, 0.76, 0.69, 0.74, 0.76, 0.66, 0.74, 0.65, 0.75, 0.75, 0.74, 0.74, 0.76, 0.78, 0.7, 0.7, 0.75, 0.71, 0.76, 0.76, 0.75, 0.76, 0.76, 0.73, 0.73, 0.7, 0.74, 0.75, 0.75, 0.74, 0.74, 0.75, 0.69, 0.73, 0.72, 0.77, 0.77, 0.75, 0.75, 0.73, 0.69, 0.69, 0.75, 0.76, 0.77, 0.77, 0.73, 0.7, 0.7, 0.7, 0.78, 0.78, 0.76, 0.76, 0.71, 0.71, 0.74, 0.77, 0.74, 0.74, 0.76, 0.76, 0.75, 0.75, 0.76, 0.68, 0.76, 0.76, 0.68, 0.76, 0.7, 0.65, 0.7, 0.77, 0.78, 0.72, 0.74, 0.75, 0.65, 0.75, 0.77, 0.71, 0.71, 0.76, 0.77, 0.71, 0.71, 0.73, 0.77, 0.65, 0.75, 0.73, 0.75, 0.73, 0.68, 0.72, 0.72, 0.76, 0.76, 0.75, 0.72, 0.65, 0.75, 0.75, 0.73, 0.76, 0.74, 0.73, 0.75, 0.69, 0.69, 0.69, 0.69, 0.76, 0.78, 0.69, 0.75, 0.71, 0.7, 0.76, 0.67, 0.72, 0.76, 0.73, 0.66, 0.72, 0.69, 0.73, 0.75, 0.69, 0.74, 0.75, 0.73, 0.69, 0.74, 0.69, 0.69, 0.75, 0.74, 0.7, 0.75, 0.69, 0.7, 0.74, 0.76, 0.73, 0.75, 0.76, 0.74, 0.76, 0.76, 0.75, 0.71, 0.74, 0.72, 0.75, 0.7, 0.73, 0.76, 0.74, 0.75, 0.75, 0.71, 0.7, 0.69, 0.69, 0.69, 0.72, 0.74, 0.76, 0.74, 0.73, 0.7, 0.76, 0.68, 0.72, 0.75, 0.65, 0.69, 0.76, 0.68, 0.76, 0.76, 0.74, 0.73, 0.68, 0.75, 0.69, 0.76, 0.75, 0.69, 0.69, 0.69, 0.76, 0.76, 0.76, 0.69, 0.74, 0.65, 0.75, 0.76, 0.76, 0.67, 0.75, 0.76, 0.74, 0.74, 0.74, 0.73, 0.75, 0.73, 0.72, 0.69, 0.74, 0.7, 0.71, 0.71, 0.71, 0.76, 0.72, 0.71, 0.71, 0.68, 0.76, 0.76, 0.72, 0.72, 0.74, 0.73, 0.66, 0.69, 0.73, 0.75, 0.69, 0.75, 0.73, 0.71, 0.75, 0.75, 0.72, 0.75, 0.76, 0.76, 0.76, 0.74, 0.7, 0.73, 0.75, 0.67, 0.67, 0.71, 0.76, 0.76, 0.69, 0.68, 0.76, 0.72, 0.76, 0.7, 0.68, 0.73, 0.72, 0.7, 0.68, 0.72, 0.76, 0.76, 0.76, 0.7, 0.69, 0.69, 0.73, 0.71, 0.78, 0.65, 0.76, 0.73, 0.76, 0.74, 0.65, 0.76, 0.73, 0.72, 0.75, 0.73, 0.7, 0.73, 0.76, 0.67, 0.73, 0.71, 0.75, 0.75, 0.75, 0.77, 0.68, 0.67, 0.78, 0.7, 0.76, 0.74, 0.75, 0.75, 0.74, 0.69, 0.7, 0.76, 0.75, 0.68, 0.7, 0.73}; //Pressure shift coeff. const float delta[460] = {-0.002524, -0.002951, -0.002956, -0.002924, -0.002834, -0.002755, -0.003016, -0.002235, -0.002919, -0.002834, -0.00311, -0.002235, -0.002594, -0.00309, -0.00311, -0.003324, -0.001768, -0.002627, -0.002876, -0.002876, -0.002897, -0.002884, -0.002387, -0.002387, -0.003621, -0.002328, -0.003187, -0.002294, -0.003509, -0.002551, -0.002294, -0.002917, -0.002917, -0.002915, -0.002551, -0.003711, -0.003049, -0.003277, -0.002489, -0.002177, -0.00297, -0.00235, -0.002323, -0.002323, -0.002918, -0.002891, -0.002177, -0.002876, -0.00235, -0.002872, -0.00262, -0.002887, -0.002887, -0.002876, -0.002513, -0.001719, -0.00262, -0.002876, -0.00224, -0.002522, -0.001776, -0.001776, -0.002914, -0.002914, -0.003201, -0.002257, -0.002257, -0.002915, -0.002611, -0.00265, -0.00301, -0.002069, -0.003084, -0.003084, -0.00301, -0.002732, -0.002551, -0.002551, -0.002189, -0.002894, -0.00272, -0.002741, -0.00331, -0.00331, -0.003107, -0.003346, -0.003091, -0.003091, -0.003077, -0.002185, -0.002185, -0.003027, -0.003027, -0.002974, -0.002876, -0.002931, -0.002741, -0.003208, -0.003016, -0.003017, -0.002557, -0.002884, -0.002888, -0.002182, -0.002392, -0.003124, -0.002884, -0.002294, -0.002933, -0.00298, -0.002828, -0.002107, -0.002107, -0.002304, -0.002544, -0.00298, -0.002961, -0.003049, -0.002924, -0.002985, -0.002756, -0.003404, -0.003049, -0.00329, -0.002911, -0.003648, -0.002294, -0.002294, -0.002985, -0.002914, -0.002037, -0.002037, -0.002911, -0.002924, -0.002041, -0.003046, -0.002262, -0.003301, -0.001802, -0.00188, -0.001802, -0.002894, -0.003016, -0.001977, -0.001977, -0.003134, -0.002814, -0.003134, -0.002891, -0.002732, -0.002891, -0.003277, -0.002958, -0.002904, -0.003479, -0.002958, -0.003736, -0.002897, -0.002933, -0.001926, -0.001926, -0.002894, -0.001818, -0.002172, -0.002218, -0.002869, -0.002112, -0.002917, -0.002917, -0.002925, -0.001884, -0.001884, -0.002808, -0.002167, -0.00317, -0.00193, -0.002956, -0.002951, -0.002828, -0.002828, -0.00296, -0.003224, -0.002788, -0.003063, -0.001849, -0.001849, -0.00289, -0.00289, -0.002808, -0.002509, -0.001758, -0.002954, -0.002905, -0.001815, -0.001815, -0.001981, -0.003171, -0.002172, -0.002172, -0.001767, -0.001767, -0.002011, -0.002923, -0.002691, -0.00309, -0.002849, -0.001853, -0.002849, -0.002334, -0.0029, -0.001888, -0.002884, -0.002884, -0.002905, -0.003331, -0.00292, -0.00292, -0.003331, -0.002929, -0.002283, -0.004054, -0.002633, -0.001819, -0.001771, -0.002753, -0.001805, -0.002057, -0.003676, -0.002057, -0.001608, -0.003098, -0.003098, -0.002891, -0.001927, -0.00311, -0.00311, -0.003024, -0.001927, -0.003603, -0.00292, -0.003024, -0.002861, -0.003003, -0.003374, -0.003043, -0.003043, -0.002885, -0.002885, -0.002884, -0.00309, -0.003759, -0.002884, -0.002258, -0.002836, -0.002902, -0.002991, -0.003033, -0.002935, -0.00179, -0.002611, -0.002605, -0.003229, -0.001741, -0.001864, -0.002605, -0.002946, -0.003148, -0.002283, -0.00292, -0.003432, -0.003063, -0.002923, -0.002997, -0.003451, -0.003063, -0.002414, -0.00304, -0.002247, -0.002557, -0.002997, -0.002247, -0.002997, -0.002414, -0.002946, -0.002252, -0.002095, -0.002951, -0.002997, -0.003157, -0.00293, -0.002252, -0.003157, -0.00224, -0.002888, -0.002762, -0.002943, -0.002888, -0.002987, -0.0029, -0.002902, -0.00293, -0.002734, -0.002843, -0.002753, -0.002299, -0.002686, -0.002762, -0.002897, -0.002852, -0.002299, -0.00292, -0.003124, -0.002172, -0.002605, -0.002605, -0.003249, -0.003072, -0.002974, -0.001749, -0.002974, -0.002776, -0.003153, -0.001749, -0.003324, -0.003077, -0.002936, -0.003703, -0.002345, -0.002891, -0.003359, -0.002897, -0.002897, -0.002971, -0.003046, -0.003359, -0.002943, -0.002568, -0.002914, -0.00296, -0.002568, -0.002345, -0.002345, -0.00292, -0.00292, -0.002894, -0.002584, -0.00284, -0.003786, -0.002956, -0.002892, -0.002927, -0.003404, -0.002926, -0.003016, -0.002843, -0.002843, -0.00284, -0.001876, -0.00287, -0.001876, -0.002753, -0.002532, -0.002834, -0.002706, -0.001967, -0.003134, -0.003134, -0.002897, -0.003019, -0.003117, -0.003117, -0.003374, -0.002894, -0.002894, -0.003057, -0.003057, -0.002834, -0.002814, -0.003425, -0.003252, -0.00304, -0.002926, -0.002247, -0.002926, -0.00304, -0.002709, -0.002929, -0.002863, -0.003049, -0.002863, -0.003014, -0.002888, -0.002888, -0.002946, -0.003171, -0.003003, -0.00293, -0.003329, -0.003457, -0.003105, -0.002873, -0.002884, -0.00179, -0.003346, -0.002897, -0.003077, -0.0029, -0.003177, -0.003324, -0.003011, -0.003077, -0.003177, -0.003274, -0.003054, -0.002885, -0.002885, -0.002873, -0.002669, -0.002247, -0.002247, -0.003011, -0.002171, -0.001741, -0.003728, -0.002888, -0.002183, -0.002888, -0.002823, -0.003816, -0.002927, -0.00301, -0.003077, -0.002932, -0.00301, -0.003135, -0.002348, -0.002892, -0.003389, -0.00188, -0.003091, -0.002876, -0.002923, -0.002932, -0.001931, -0.002624, -0.003389, -0.00173, -0.002644, -0.002887, -0.002991, -0.00296, -0.002949, -0.002991, -0.002509, -0.002644, -0.002887, -0.00293, -0.003265, -0.003208, -0.002848};
Observation: Please check the post at Jan 24, 2018 9:05 AM in this post e2e.ti.com/support/microcontrollers/c2000/f/171/t/654370
I assume that when the program goes into function 'lorlineshape()' then the program is not getting enough memory from the sectors created in the default linking files. and thus there are garbage results.
My Question:
Can anyone tell when the main function calls 'lorlineshape()' then the variables which are initialized/declared in this function acquire which space in the memory?
and when the program comes out of the function then this space is released or not? and since I am calling this function in the loop in original program, then does the function acuire new space each time the function is called? how does this work? is there a documentation to read or someone to explain.
Thank for the patient to read till the end.
Thanks in advance for any help you provide
Regards,