Tool/software: Code Composer Studio
Hello, my friend, I have met a problem when I run the program 'HVPM_Sensorless_2833x' in FLASH. The program will restart to "codestart" when it meet the function ADC_cal(). However, if the ADC_cal() is commented out, everything is ok.
Here are my configurations:
1. GPIO84/GPIO85/GPIO86/GPIO87 are all connected to 3.3V;
2. Using F28335_FLASH_HVPM_Sensorless.cmd;
3. Add "FLASH" macro in the predefined symbols page of project properties;
4. CPU Frequency 150MHZ, core voltages are 3.3V and 1.9V;
5. Watchdog is not used;
Moreover, if I run the program in RAM using F28335_RAM_HVPM_Sensorless.cmd, everything is ok.