Please give us any feedback or solution of below symptoms for the P/N called TMS320F28335
- Symptoms
: P/N = DSP28335 occurs booting defection while it is on boot at low temperature environment between 0 to -32`C.
- Local state of the DSP board during boot at low temperature.
: Power 3.3V, 1.9V Normal, Reset Normal(same as normal temperature boot)
- Environmental factors on DSP
: CCS version 3.3.82.13
BIOS Version 5.41.10.36
Code Generation version 5.2.11
- Phenomenon at failure occurrence while boot.
: During initializing DSP in program, error appears function of InitXintF(); Unable to boot as it appears endless loop during initializing on local area.
- History
: No issue or any defective error on production between 2015~2016, initial issue on 2017, most of the board we made in 2018 had continual symptoms(error occurrence).
Also, same type of other board have same symptoms.
In our perspective, we estimate that the firmware implemented in the DSP BIOS occurs this typical symptoms. It seems there must have been upgrade on other function or function of the DSP chip itself as this symptoms came out so suddenly at some point.
In summary, as there were no issue or any defective error occurred with the previous DSP Board we made in 2015~2016. At this point, we would like to ask you to review this DSP itself precisely.
Q1) Is there any relevant inquiry facing similar situation as ours?
Q2) Occurs only in BIOS Version?
Q3) Which part would we consider to review?
Or if you could possibly arrange the schedule to support by ourselves, that would be so appreciatable.