Other Parts Discussed in Thread: DRV8301
Hello everyone,
I wondering if anyone has come across the following issue with the PWM outputs on the F28035: I can power up my board and get really weak signals (mV range) on my PWM pins. However, the PWM outputs have LED indicators connected to them and are lighting up in the sequence I have programmed them to do. I also have a switch that I am using to Increase the duty cycle and another switch I am using to decrease the duty cycle. When I use the switches to change the duty cycles, the LEDs respond as expected but with the same low mV range voltage. However, if I hit the reset button on my board, the MCU comes back on and the PWM signals are operating in the expected voltage range. If anyone has had such a problem with the PWM outputs, could you please enlighten me. I have tried to figure this out for a while. The only thing I can think of that would cause this problem is that the MCU is bad. If so, have any of you had any experience where the PWM causes the MCU to get damaged? I am afraid this might be a layout issue with the board as well but not sure. Thank you.
-Brandon