Part Number: DRV8301-69M-KIT
Other Parts Discussed in Thread: DRV8301
Hey TI,
I have a few questions again.
1. Is it possible to use lab11e with current control instead of speed control?
If yes, what do I have to change?
2. I’m very interested in how one can limit the rpm in current control mode? I’ve searched about few threads, but I didn’t find an answer.
3. I added a current ramp in lab5a because my motor was stuttering/jerking if I increased iqref_A too fast.
But that wasn’t the problem, as I know now. It’s still the same behaviour with or without ramp.
Until 60A it works perfectly, but when iqref_A is between 60 and 80 ampere the motor begins hard stuttering/jerking.
The first thing I thought of was that I had not used enough load. Because of that I tried driving uphill but still the same behaviour. Different Kp and Ki did not change anything either.
Do you have any ideas what that could be?
I read in a thread that the Ls is maybe changing when high current flows. Would this be a possibility?
The motor specs are 50V 80A and I use the drv8301 kit(my own hw is not finished as of yet).
I changed the current scaling to 1mohm and the board is cooled.
also I have to say I’m happy with Instaspin. My vehicle is working quite well already.
thanks in advance