Hi --
I have inherited some schematics from a previous colleague which show VREGENZ connected to GND and VDD pins bypassed by not externally connected (see image attached). I noticed on the datasheet that VREGENZ is not supported and must be tied to VDDIO.
I have one of the boards that use the inherited schematic and I am measuring 1.2V at the VDD pins.
Was REGENZ support removed from the F28377 in the past year, or can I use the inherited schematics as is?
Thanks,
Eric