Hi @ all,
I want to use the PWM registers to actualize a signal (see figure). Which of the PWM registers I have to use?
Is it possible to configurate the PWM registers with a frequency of 25 kHz and use the deadband unit? Are there other/better oportunities to actualize this signal?
I need this signal on the GPIO0 and a complementary signal GPIO2.

With best regards,
Chris