Part Number: LAUNCHXL-F28027F
Hi
My student had some voltage issues on the connexion pins (I don't know exactly what)
but now when powering from USB / emulator it consumes 0.9A and USB voltage drops to 4.8V... then the launchpad stops working (I thing the emulator can't maintain the 3.3V )
I tried powering from an external 10V DC power through an EVM8301 that I put on TOP of the Launchpad, this way (I think that the voltage regulator 3.3V on the EVM is much powerful and maintain the voltage even if there is a large current that is thrown from the 10 DC supply : 0.5 A ! of course without any BLDC motor on the EVM )
and the F28027F gets very very hot after 2 seconds.. you can't touch it
so I cut the power, tried several times, same, there is no visible damaged parts (C5 L4 C20...) near the 27F
Do you think if I just desolder and solder another 27F, I will get the board working or I just throw away the Launchpad ?