Tool/software: Code Composer Studio
Hi
I just drop here a hardware question, i am try to use external sensor board designed by myself to provide several feedback or reference signal in order to complete a control strategy. I can see in the analog mapping there is a few spare ADCs, for example, ADCC4 and ADCC5, however, there is no connector can get access to these pins on board. There is possibility to soldering , but it is very tight soldering, will be very difficult. Just got a idea that if i can have a external connector in the intermediate stage between control card and 180 pin connector. And the connector should be able to have better soldering oppotunities. Anyone done this , or anyone got a better suggestions, please let me know.
Thank you
min