Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE
I am looking at the technical reference manual for TMS320F28004x Piccolo Microcontrollers (Literature Number: SPRUI33A).
Referring to 15.1 Buffered Digital-to-Analog Converter (DAC) Overview, which states "The buffered DAC is a general-purpose DAC that can be used to generate a DC voltage in addition to AC waveforms such as sine waves, square waves, triangle waves and so forth."
Can the AC waveforms be set up / configured via registers? I am hoping the AC waveform, such as sine or ramp, can be set up in hardware configuration to let the DAC output waveform be autonomous, rather than constantly updating the DAC value in software to create the desired AC waveform. Section 15.1 does not mention how to generate the AC waveforms.
Thank you.
Literature Number: SPRUI33A