This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TIDM-1003: Error while executing proj_lab1v.c

Intellectual 610 points

Replies: 4

Views: 383

Part Number: TIDM-1003

Hi,

I have downloaded the TIDM1003 project files and started working on Lab1b.  I get following error

1) #20 Identifier "CTRL_Mode_e" is undefined.

2) #20 identifier "CTRL_mode_Full" is undefined

3) #20 identifier "CTRL_Mode_Voltage is undefined

4) gmake [proj_lab1b] Error 1

Could you suggest how to sort this.

thx

K.V.Rao

  • Sorry its proj_lab1b.c
  • In reply to K.V. Rao:

    Please download the TIDM_1003 software from the link below, you may find the "TIDM_1003_sw.zip" in the compressive package, please extract it that including all files for TIDM-1003, it's more simple without following the section 3.2.2 in application notes.

    www.ti.com/.../TIDM-1003
  • In reply to Yanming Luo:

    Dear Yanming,

    Thanks for your response.  Actually it so happened that I was following the section 3.2.2 and copied the files to destination directory  Now what to do.  Would I need to reinstall CCS and motor ware?.

    Please suggest.

    thx & rgds

    KVRao

    .

  • In reply to K.V. Rao:

    No, you only need to use the compressive file "TIDM_1003_sw.zip" which is an independent project includes all files to support TIDM-1003 design.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.