Other Parts Discussed in Thread: C2000WARE, , TMS320F28379D
Hi,
I have few queries on the CAN BOOT and CAN flasble bootloader
1. How to enter into CAN BOOT and Exit from CAN BOOT mode if we are not using the OTP method. For now we planing to wtitten one application branching test code form there we are driectly branching to CAN boot jump address 0x03FF4FC. Is this method is correct? After this point we are loading the CAN kernal and Application.
2. Which boot comand we should have to used for genrating the ASCII file .a00? Please provide the same.
2. My important query is if CAN Kernal has erased the complete flash to load the new application and power is switched off. Then there is no applicaion in the flash in this case what will happen and how to enter into CAN BOOT Mode again after power ON? I dont have JTAG programmer to flash/program the application again? Please guide me how to handdle this kind of stiuations. We are running out of the FLASH also. we can't afford to keep one complete sector for braching program which can jump to CAN Boot.
3. Is the possible to erase the pratial sector instated of erasing the complete sector. In this case our plan is to keep the branching code at start of sector and only erase the part which are not being used.
We need this details urgently.
Regards,
Pandurang Khutal