Part Number: TMS320F28069M
Tool/software: Code Composer Studio
Attempting to flash a brand new F28069m which is fresh from the factory, using a XDS110 I have been using a DRV8301HC module, and have been using the built in XDS100 to flash that board, moved to our new board and set up a new target configuration. If I run the "Launch Selected Configuration" it launches into the debug screen and I can right click on the c28x debug probe or the cla debug probe, they connect just fine and show that the processor is set at 0x3FF75B which is in the Bootloader. When I try to run a load or an erase or a cpu reset the console outputs "Device Calibration not complete, check if device is unlocked and recalibrate.". I have no reason to believe the processor is locked as it's brand new. The hardware connection of the JTAG connection appears to be the same as on the example board, even though the processor on the controlcard is not connected to the JTAG. I have read related posts and it seems we don't share any problems with the other posts.