This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TMDSCNCD28054MISO: TMDSCNCD28054MISO

Prodigy 65 points

Replies: 4

Views: 163

Part Number: TMDSCNCD28054MISO

 Hi ,

i am using a  TMDSCNCD28054MISO controller card and i need the pin details so that i can design a system for my application kindly post the details .



  • Does any on have the GPIO details of
    TMDSCNCD28054MISO controle card if so post me the link
  • In reply to Nareshkumar bala:

    Did you checkout the schematics available in C2000Ware in the path below?

    C2000Ware>\boards\controlCARDs\TMDSCNCD28055ISO\R1_2

    ---------------------------------------------------------------------------------------------------

    If a post answers your question, please mark it with the "verify answer" button.

    Other useful links:

    C2000 Getting Started      C2000 Flash Common Issues/FAQs      Emulation FAQ

     

  • In reply to Manoj Santha Mohan:

    hi,
    i couldn't find the schematics can you share the link
  • In reply to Nareshkumar bala:

    Nareshkumar,

    you need to download and install C2000Ware. The schematics are included in that software package. You can find them at the path that Manoj has indicated above, but if that is unclear I have included a screen capture of the file on my system below.

    If you are looking for the peripheral functions on each GPIO then you can look at the Data Sheet and TRM

    Regards,
    Cody 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.