Other Parts Discussed in Thread: TMDSDOCK28035,
Hi,
Although it can be written in the API Firmware version of 01.00.07.00 on the target board equipped with F28035,
the following error occurred in 01.00.09.00, causing a problem that can not be written.
ERROR 70: DSP CLK frequency error
Because there is a problem in the environment of my customer, the following environment is used to compare
the operation due to the difference of Firmware version.
· TMDSDOCK28035
· C2000-GANG (API Firmware version 01.00.07.00 and 01.00.09.00)
· Convert out file of Example_ 28035_Flash to hex file and use it
Write once to the device, and then write it several times with the GO (F9) button.
At that time, the device is turned on.
1) In the case of 01.00.07.00
It is possible to write with GO (F9) button.
2) In the case of 01.00.09.00
The first it is possible to write.
"ERROR 70" occurs after the second time and it can not be written.
[Question]
Does Firmware of 01.00.09.00 have any changes to F2803x?
Best Regards,
Koichi