Part Number: TMS320F28069
Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
Hi,
I'm using InstaSpin foc motorware for my ACIM Motor. We identified motorparameters with the example lab2a with the hvkit_rev1p1.
My motor-rpm has to be 12'000 so 200 Hz (1 pole-pair). I've read, that the measured phase current correspond with the electrical speed of the motor. My problem is, I can not measure the real RPM of the motor external with any encoder, because the motor is a closed system.
The estimated motor speed seems to be incorrect, when compared to the phase current.
With no load, the estimator gives 12'000 RPM back, but the measured phase current with an oscilloscope shows about 215 Hz (12900 RPM)
With load on the motor its exactly the opposide. I measure about 180 Hz (10800 RPM) but the estimator gives back a value around 9000 RPM. With load I also have the problem, that the speed is decreasing, so the controller cannot control the motot correctly to the set speed.
What could cause this problem?
Another question is, how is the speed measured by the controller without any sensor? I cant find that information in any documentation.
Best regards,
Dani