This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 194
Part Number: TIDM-1003
Dear TI Experts:
For the schematic circuit of TIDM-1003, I found the THROTTLE command input.
1. The THROTTLE command input is related to speed, right? It is a DC voltage input, right? What is the DC range? -3.3V ~3.3V?
2. Why does the THROTTLE command input connect to a ADC pin and a GPIO pin? Do you have some suggestions in the s/w programming?
Thanks for your kind reply in advance.
Tang Han
Did a reply answer your question? If yes, please click the "Verify Answer" button located at the bottom of that post.Visit these helpful C2000 Links!
In reply to Sean Bigley: