This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TIDM-1003: THROTTLE command input

Intellectual 915 points

Replies: 2

Views: 195

Part Number: TIDM-1003

Dear TI Experts:

For the schematic circuit of TIDM-1003, I found the THROTTLE command input.

1. The THROTTLE command input is related to speed, right?  It is a DC voltage input, right?   What is the DC range?  -3.3V ~3.3V? 

2. Why does the THROTTLE command input connect to a ADC pin and a GPIO pin?  Do you have some suggestions in the s/w programming?

Thanks for your kind reply in advance.

Tang Han

  • 1) The throttle input can be assigned to any reference you'd like, such as speed. The input range is 0-3.3V that can be varied with the external potentiometer

    2) the throttle can be set to input to either an ADC pin, or an ECAP pin that is muxed with GPIO19

    Sean

    Did a reply answer your question? If yes, please click the "Verify Answer" button located at the bottom of that post.
    Visit these helpful C2000 Links!

    C2000 TI Wiki Pages
    TI Forum Sitemap
    ControlSUITE
    C2000 Getting Started
    CLA FAQs
    Workshop Material!
  • In reply to Sean Bigley:

    Dear Sean:

    Thanks for your kind and professional reply.

    ^_^
    Wish you the best!
    Tang Han

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.