Other Parts Discussed in Thread: TMDSCNCD280049C, TMDSADAP180TO100
Can DRV8312-69M-KIT be used with 280049 control card(TMDSCNCD280049C) for InstaSPIN evaluation?
If there are any limitation, please let me know.
Regards,
Furuya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can DRV8312-69M-KIT be used with 280049 control card(TMDSCNCD280049C) for InstaSPIN evaluation?
If there are any limitation, please let me know.
Regards,
Furuya
Hi Furuya-san,
The F280049C controlCARD should be able to physically plug into the DRV8312-69M-KIT, if the TMDSADAP180TO100 is used. It appears that, if done, the F280049C MCU will have its peripherals in the right place that utilize the majority, if not all, of the features of the board.
However, from a software perspective, there will not be any software that uses this configuration. As such, you/customer would need to write software that would make the system work. This may be a bit challenging.
Note that InstaSPIN with the F28004x series is not currently supported:
https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/740747
Thank you,
Brett
Furuya-san,
Instaspin is typically used with BLDC motors(Brush-less Direct Current motors).
The link you sent was for a brushed motor(ブラシ付モータ) correct? Below is a link that talks about some of the potential draw backs of using a brushed motor with instaSPIN.
C2000 can certainly drive a brushed motor without instaSPIN. However the kit referenced above was designed to work with BLDC motors.
Regards,
Cody