Part Number: LAUNCHXL-F280049C
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hello, I've recently bought a Launchxl- F280049c launchpad from TI. I am trying to Flash example code from C2000-device support present in C2000ware but I am unable to do so.
I am getting the following error-
The version of CSS installed---- Version: 8.3.0.00009
I've tried to Test the connection from VERIFY option in properties and got the following script.-
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the XDS110 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for XDS110 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
[End]
would like to know, how I can repair this error!. Is my Board damaged??
Regards,
Archit