Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Good morning,
i'd like to implement a custom bootloader on my F280049C controlCARD via SCI.
To do practice with the bootloader concepts and the examples provided by TI, I’m trying to do an exercise.
I’m going to use the “flashapi_ex2_sci_kernel” example (BANK0_NO_LDFU build configuration) and the “serial_flash_programmer” PC application available in the C2000Ware software pack.
I set the “flash” boot mode from Bank 0 and Sector 0. In the sectors 0, 1 and 2 of Bank 0 I stored the SCI kernel (SCI bootloader).
The BANK0_NO_LDFU kernel configuration must be used to manipulate flash in Bank 1 so I built the “flashapi_ex3_live_firmware_update” example (BANK1_FLASH build configuration) with the purpose to use the “flashapi_ex3_live_firmware_updateBANK1FLASH.txt” file generated as Application code. In the picture above is shown what I’m going to do.
When I run the firmware download with the console command “serial_flash_programmer.exe -d f28004x -k flashapi_ex2_sci_kernel.txt -a flashapi_ex3_live_firmware_updateBANK1FLASH.txt -b 9600 -p COM1 -v -w” I receive always the same “crash” during the download.
The “serial flash programmer” tries to download the kernel. Maybe it’s configured to work with the SCI bootloader stored in the ROM memory. This step is not required in my example because I boot directly from Bank 0 and Sector 0 where the SCI kernel is stored.
I’d like to ask you:
- Is it possible to disable the kernel download in the “serial flash programmer”? If yes, in which way?
- Is my idea correct or there is some concepts wrong?
Thank you very much for your support.
Fabrizio