Part Number: DRV8301-HC-C2-KIT
Tool/software: Code Composer Studio
Dear Sir/Madam-
I have a need to demonstrate BLDC technology on the DRV830x-HC-C2-KIT_v105 kit to compare it with newer PMSM technology. I have operated the BLDC_Sensorless software on the DRV8312-C2-KIT_v128 kit and it works just fine. When the software is downloaded to the DRV830x-HC-C2-KIT_v105 hardware, and when scope probes are used to examine PWM_AH, PWM_AL PWM_BH, PWM_BL, and PWM_CH, PWM_CL channels, the appropriate PWM are present. However, once moving to lab2 and examining ADC-Vhb1, ADC-Vhb2, and ADC-Vhb3 there is no signal and of course the connected motor won't spin or even lock-up. There must be some simple fix? Before you give me your standard TI party line, "BLDC_Sensorless is not supported..." - consider the immortal words of George Santayana, "Those who cannot remember the past are condemned to repeat it." there are historical reasons why the motor control experts evolved to the Clarke/Park methodology, there are many motor controller still using BLDC, not being able to explain to your customers why the new way is better than the old way will increase your profits.
Thanks,
Kurt Kloesel