Other Parts Discussed in Thread: SFRA
Tool/software: Code Composer Studio
Hi Champs,
I have some problems when doing psfb topology by peak current mode control.
The PWM switching frequence is about 47KHz, and using type III compensator.
When closed-loop gain and BW is very small, output(Vo_blue line) at full & half loads is stable, and there are some small ringing at light loads(10%).
After adjust the compensator to increase the bandwidth to 500Hz, the amplitude and range of output ringring at light loads become larger(1%~20%).
I want to know the reason for the output ringing, because of the compensator or somthing else.
Would you kindly help to suggest how to solve or improve this problem?
Thanks.
Regard,