This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDSCNCD28335: JTAG header for TMDSRSLVR resolver and TMDSCNCD28335 dev kit

Part Number: TMDSCNCD28335

Tool/software: Code Composer Studio

I would like to try to do CCS 8.0 development using a Blackhawk debug probe with a TMDSCNCD28335 development kit.      The resolver being used is 'TMDSRSLVR'.  I had through the 20 pin connector on the resolvr was JTAG but it turns out it is SPI?  is this correct?

So is there another resolver that can be used that has JTAG with the TMDSCNCD28335