Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, SYSBIOS
Tool/software: TI-RTOS
Hi,
I want to implement a little SYS/BIOS and C2000Ware project that prints in console a char received by SCI comms. And I want to configure an RX SCI interruption. In the meantime, there are 2 tasks which simply print through console, every second, a string. To do so, I have integrated driverlib into the SYS/BIOS project. And I have copied big part of the code found in driverlib sci loopback interrupts example.
My code is as follows:
#include <xdc/std.h>
#include <xdc/runtime/Error.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include "c2000ware/device.h"
#define TASK_SCI_BASE SCIB_BASE
Void task1(UArg arg1, UArg arg2);
/* Counter incremented by timer interrupt */
volatile UInt tickCount = 0;
/*
* ======== main ========
*/
Int main()
{
Task_Params task_prms;
Error_Block eb;
/*
* Print "Hello world" to a log buffer.
*/
System_printf("START\r\n");
System_flush();
Error_init(&eb);
Task_Params_init(&task_prms);
task_prms.stackSize = 1024;
task_prms.priority = 15;
Task_create(task1, &task_prms, &eb);
/*
* Start BIOS.
* Begins task scheduling.
*/
BIOS_start(); /* does not return */
return(0);
}
//
// sciaRXFIFOISR - SCIA Receive FIFO ISR
//
__interrupt void sciRXFIFOISR(void)
{
uint16_t a[10];
SCI_readCharArray(TASK_SCI_BASE, a, 1);
a[1] = '\0';
System_printf("a = %s\r\n", a);
System_flush();
SCI_clearOverflowStatus(TASK_SCI_BASE);
SCI_clearInterruptStatus(TASK_SCI_BASE, SCI_INT_RXFF);
// Issue PIE ack
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}
void initComms(void) {
//
// Initialize device clock and peripherals
//
Device_init();
//
// Setup GPIO by disabling pin locks and enabling pullups
//
Device_initGPIO();
//
// GPIO28 is the SCI Rx pin.
//
GPIO_setMasterCore(71, GPIO_CORE_CPU1);
GPIO_setPinConfig(GPIO_71_SCIRXDB);
GPIO_setDirectionMode(71, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(71, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(71, GPIO_QUAL_ASYNC);
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
Interrupt_register(INT_SCIB_RX, sciRXFIFOISR);
//
// 8 char bits, 1 stop bit, no parity. Baud rate is 9600.
//
SCI_setConfig(TASK_SCI_BASE, DEVICE_LSPCLK_FREQ, 115200, (SCI_CONFIG_WLEN_8 |
SCI_CONFIG_STOP_ONE |
SCI_CONFIG_PAR_NONE));
SCI_enableModule(TASK_SCI_BASE);
SCI_resetChannels(TASK_SCI_BASE);
SCI_enableFIFO(TASK_SCI_BASE);
//
// RX and TX FIFO Interrupts Enabled
//
SCI_enableInterrupt(TASK_SCI_BASE, SCI_INT_RXFF);
SCI_disableInterrupt(TASK_SCI_BASE, SCI_INT_RXERR);
SCI_setFIFOInterruptLevel(TASK_SCI_BASE, SCI_FIFO_TX0, SCI_FIFO_RX1);
SCI_performSoftwareReset(TASK_SCI_BASE);
SCI_resetTxFIFO(TASK_SCI_BASE);
SCI_resetRxFIFO(TASK_SCI_BASE);
#ifdef AUTOBAUD
//
// Perform an autobaud lock.
// SCI expects an 'a' or 'A' to lock the baud rate.
//
SCI_lockAutobaud(TASK_SCI_BASE);
#endif
Interrupt_enable(INT_SCIB_RX);
Interrupt_enable(INT_SCIB_TX);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
//
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
//
EINT;
ERTM;
}
Void task2(UArg arg1, UArg arg2) {
initComms();
while (TRUE) {
System_printf("Task 2\r\n");
System_flush();
Task_sleep(1000);
}
}
Void task1(UArg arg1, UArg arg2) {
Task_Params task_prms;
Error_Block eb;
Error_init(&eb);
Task_Params_init(&task_prms);
task_prms.stackSize = 1024;
task_prms.priority = 15;
Task_create(task2, &task_prms, &eb);
while (TRUE) {
System_printf("Task 1\r\n");
System_flush();
Task_sleep(1000);
}
}
The problem is that the tasks which print a simple string each second get both stucked at instruction:
Task_sleep(1000);
And if I comment next line, they don't get stuck:
initComms();
Debugging, I have checked that within initComms() function the function which makes the 2 other tasks not work is:
Interrupt_initModule();
And I have checked the code of this function and the next lines are responsible for getting the other 2 tasks stucked at Task_sleep() function:
IER = 0x0000U; IFR = 0x0000U;
I guess this driverlib code is conflictive with my app.cfg, so please find it bellow:
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Error = xdc.useModule('xdc.runtime.Error');
var Log = xdc.useModule('xdc.runtime.Log');
var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
var Main = xdc.useModule('xdc.runtime.Main');
var Memory = xdc.useModule('xdc.runtime.Memory')
var SysMin = xdc.useModule('xdc.runtime.SysMin');
var System = xdc.useModule('xdc.runtime.System');
var Text = xdc.useModule('xdc.runtime.Text');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
var Swi = xdc.useModule('ti.sysbios.knl.Swi');
var Task = xdc.useModule('ti.sysbios.knl.Task');
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
var Hwi = xdc.useModule('ti.sysbios.family.c28.Hwi');
var Boot = xdc.useModule('ti.catalog.c2800.initF2837x.Boot');
/*
* Uncomment this line to globally disable Asserts.
* All modules inherit the default from the 'Defaults' module. You
* can override these defaults on a per-module basis using Module.common$.
* Disabling Asserts will save code space and improve runtime performance.
Defaults.common$.diags_ASSERT = Diags.ALWAYS_OFF;
*/
/*
* Uncomment this line to keep module names from being loaded on the target.
* The module name strings are placed in the .const section. Setting this
* parameter to false will save space in the .const section. Error and
* Assert messages will contain an "unknown module" prefix instead
* of the actual module name.
Defaults.common$.namedModule = false;
*/
/*
* Minimize exit handler array in System. The System module includes
* an array of functions that are registered with System_atexit() to be
* called by System_exit().
*/
System.maxAtexitHandlers = 4;
/*
* Uncomment this line to disable the Error print function.
* We lose error information when this is disabled since the errors are
* not printed. Disabling the raiseHook will save some code space if
* your app is not using System_printf() since the Error_print() function
* calls System_printf().
Error.raiseHook = null;
*/
/*
* Uncomment this line to keep Error, Assert, and Log strings from being
* loaded on the target. These strings are placed in the .const section.
* Setting this parameter to false will save space in the .const section.
* Error, Assert and Log message will print raw ids and args instead of
* a formatted message.
Text.isLoaded = false;
*/
/*
* Uncomment this line to disable the output of characters by SysMin
* when the program exits. SysMin writes characters to a circular buffer.
* This buffer can be viewed using the SysMin Output view in ROV.
SysMin.flushAtExit = false;
*/
/*
* The BIOS module will create the default heap for the system.
* Specify the size of this default heap.
*/
BIOS.heapSize = 0x1000;
/*
* Build a custom SYS/BIOS library from sources.
*/
BIOS.libType = BIOS.LibType_Custom;
/* System stack size (used by ISRs and Swis) */
Program.stack = 0x100;
/* Circular buffer size for System_printf() */
SysMin.bufSize = 0x200;
/*
* Create and install logger for the whole system
*/
var loggerBufParams = new LoggerBuf.Params();
loggerBufParams.numEntries = 32;
var logger0 = LoggerBuf.create(loggerBufParams);
Defaults.common$.logger = logger0;
Main.common$.diags_INFO = Diags.ALWAYS_ON;
System.SupportProxy = SysMin;
Boot.configureClocks = true;
Boot.configureFlashController = true;
BIOS.cpuFreq.lo = 200000000;
Clock.tickPeriod = 1000;
Boot.SYSCLKDIVSEL = 1;
Boot.OSCCLK = 20;
Boot.SPLLIMULT = 20;
Boot.SPLLFMULT = Boot.Fract_0;
Boot.OSCCLKSRCSEL = Boot.OscClk_XTAL;
Boot.disableWatchdog = true;
Boot.bootFromFlash = true;
Boot.configSharedRAMs = true;
Can anyone tell me what is going on and propose me solutions?
Thanks in advance!
Best regards,
Adria