Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28069M
Tool/software: Code Composer Studio
Hi,
I am trying to work with the LAUNCHXL-F28379D driving the Digita Power Booster pack, But i seem to be running into some issue.
I am able to load the program into the controller ( the buck converter example Buck_VMC__F283xS) but upon running the code, The code doesnt seem to be doing anything. I am not getting any readings From the DPS, not even for the input Voltage. I have enabled Real time mode but I still cannot read anything. ideally i should at
It seems like there is no communication between the DPS and the Launchpad, because ideally, after running the code I should at least be able to get a reading of the input DC voltage in the booster Pack.
Any help will be appreciated.
%%Kudra%%