Team,
-We have today the below C2000 Tools to help with IEC60730 compliance:
http://www.ti.com/tool/C2000-SAFETI-DIAGNOSTICS-LIB
http://www.ti.com/tool/iec60730swpackages
Provided that an application should be able to achieve SIL2 requirements of the Cenelec EN50129/EN50128 railway regulation:
-Can this be achieved by the C2000 Software with the C2000 TI SW package TI provides?
-Or some HW changes are required? is an additional MCU required (like TMS570)?
-Do we have a concept of Safety application using both TMS570 and C2000 that could be potentially used for railway traction?
Thanks in advance,
A.