This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379S: pwm12 mux2 not output

Part Number: TMS320F28379S

Tool/software: Code Composer Studio

Dear all,

I working with TMS320F28379SZWT micro controller and PWM output signals.

I am able to output the pwm1a (on GPIO0), pwm1b (GPIO1) and so on to the pwm8b (on PGIO15), and it works fine.

here the code for pwm6:

  GpioCtrlRegs.GPAPUD.bit.GPIO10 = 1;    // Disable pull-up on GPIO10 (EPWM6A)
  GpioCtrlRegs.GPAPUD.bit.GPIO11 = 1;    // Disable pull-up on GPIO11 (EPWM6B)
  GpioCtrlRegs.GPAMUX1.bit.GPIO10 = 1;   // Configure GPIO8  as EPWM6A
  GpioCtrlRegs.GPAMUX1.bit.GPIO11 = 1;   // Configure GPIO9 as EPWM6B

The problem appears when I try to use the pwm on GPIO22. I not able to output the pwm12 on GPIO22.

I thing that the problem is related to GPAGMUX2

Can someone help me ?

thanks

Regards