I'm planning a design based on the 280049C for which BISS/EnDat ist mandatory.
Curently I'm working on the first schematics.
Within the other thread I learned that the position manager lib for this device is not available until now.
So for me the following questions arise:
a) Will the position manager lib for the 280049C support BISS / EnDat as advertised (and with the current silicon revision)?
b) Which resources will be used?
c) Which IOs are in use, is there already a schematic I can include to do the layout of the first sample (...and work on the other SW I need to implement).
d) What's the release date of the Pos. Manager SW lib?
Thanks & best regards,
Carl