Part Number: TMS320F28379D
Hi,
i've been browsing through the ADC characteristics has been declared on TMS320F28379D datasheet whereby single-ended conversion support was only available for 12-bit mode only. Both datasheet Table 3-1 & Section 5.10.1 has it written on it. Hence i would like to check if i need a 16-bit single ended conversion is it possible to realize using this chipset? Else may i know what are the options which i can look at which offers 4x independent ADC within single chip which is capable of 16-bit single ended signal conversion? Please advise. Thanks.
Regards,
Leo