Part Number: DRV8312-69M-KIT
1. Is it possible to remove M1?
2. Is it possible to remove RSTC,RSCB,RSCA?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8312-69M-KIT
1. Is it possible to remove M1?
2. Is it possible to remove RSTC,RSCB,RSCA?
1. I think it is possible to remove the RSTC toggle switch and DSP pin apply 3.3V directly to drv RESETA pin. Is this right?
2. When is normal op applied? Is normal op necessary?
3. I think it is possible to remove the M1 and drv M1 pin connect AGND. Is this right?
4. I have seen drv8312 evm HW guide. The guidebook says as follows:
Mode jumper "M1" - DRV8312 mode can be set to select between cycle by cycle current limit or latched overcurrent.
What's "latched overcurrent" here?
The guidebook says as follows:
M1 is in the "H" position.
1. If M1 is "H" position, I wonder if M1 is connected to AGND or VREG.
2. I read the datasheet and guide. but i don't know. When is normal op applied?
"Normal OP mode will disable control from the MCU and enable the half bridge outputs."
What does this mean? Is this necessary?