This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: CAN Flash Kernel

Part Number: TMS320F28069M
Other Parts Discussed in Thread: C2000WARE

Hi,

I recently noticed the CAN flash kernel in C2000ware and also saw a brief thread on it

https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/785489

We would need to setup a test to duplicate the functionality. Which F28069M based HW was used to validate the CAN flash kernel?

Which additional CAN HW was used on the Host side to get a CAN interface?

Similar to the SCI boot flashing, is there a Host side application available to test with?

Thanks,

--Gunter