This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] TMS320F280049C: TIDM-02002 CLLLC vs CLLC

Mastermind 38345 points

Replies: 1

Views: 669

Part Number: TMS320F280049C

What are the differences in architecture between CLLLC and CLLC ? Why choose one over the other. 

  • Instead of me acting as a translator, I will recommend the customer look at the following thesis

    vtechworks.lib.vt.edu/.../77686

    CLLLC and CLLC can be designed to be the same for the converter, however a closed form solution from CLLLC -> CLLC is required.

    The additional L on the secondary side is an easy way to get better control/degree of freedom on the switching frequency in the reverse power flow mode. It is feasible to reduce CLLLC -> CLLC however I was unable to perform a closed-loop solution to this issue. Also for high-frequency CLLLC because of use of planar magnetics and increasingly PCB winding transformer the L on sec comes naturally and is not an issue to design.

    -Manish Bhardwaj

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.