Other Parts Discussed in Thread: CONTROLSUITE,
Tool/software: Code Composer Studio
I am using proj_lab07a.(f28069m)
I'm going to add a controlsuite example code.
I added the following code.
void main(void)
{
/////////////////////////////190403
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2806x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initalize GPIO:
// This example function is found in the F2806x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
// Setup only the GP I/O only for SPI-A functionality
InitSpiGpio();
InitMcbspaGpio();
EALLOW;
GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 0;
GpioCtrlRegs.GPADIR.bit.GPIO31 = 1;
GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0;
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;
EDIS;
// Step 3. Initialize PIE vector table:
// Disable and clear all CPU interrupts
DINT;
IER = 0x0000;
IFR = 0x0000;
// Initialize PIE control registers to their default state:
// This function is found in the F2806x_PieCtrl.c file.
InitPieCtrl();
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2806x_DefaultIsr.c.
// This function is found in F2806x_PieVect.c.
InitPieVectTable();
///////////////////////////////190403
When I build, an error occurs as follows: