Part Number: TMS320F28375D
Tool/software: TI C/C++ Compiler
I came across strange behavior again...
I'm using an old C2000 compiler, TI v6.2.8.
I set two structures to CLARAM area using DATA_SECTION pragma for data exchange between CPU and CLA.
And I copied data at CPURAM to a structure member at CLARAM.
But one menber of structure wasn't copied.
C source code is like below.
[C source]
#pragma DATA_SECTION(rd_cpu1, "CLARAM");
#pragma DATA_SECTION(wr_cpu1, "CLARAM");
wr_cpu1.menber11 = A;
wr_cpu1.menber14 = B;
wr_cpu1.menber19 = C;
wr_cpu1.menber13 = D;
This is very simple code, but copy to member19 is failed. So I checked assembly code.
[Assembly source]
MOV PL, _A
MOV T, _B
MOV PH, _D
MOV AH,_C
...
MOVW DP,#_wr_cpu1+11
MOV @_wr_cpu1+11,P
MOV @_wr_cpu1+14,T
MOV @_wr_cpu1+19,AH
MOVH @_wr_cpu1+13,P
...
This also looks right, but it didn't work correct.
So I executed assembly code step by step on targe device using CCS debug.
At that time I found the cause of this abnormality in disassembly view.
[Disassembly view]
00b611: 761F020F MOVW DP, #0x20f
00b613: 3F39 MOV @0x39, P
00b614: 213C MOV @0x3c, T
00b615: 9701 MOV @0x1, AH
00b616: 573B MOVH @0x3b, P
Member19 has an offset 19 word from top of structure.
But in above code, offset of member19 is 1.
and offsets of other members is wrong too.
Result of execute of row 00b615 above code, _rd_cpu1.member1 was overwrited by content of AH.
I checked .map file and an absolute address of structure in CCS Expressions view.
[map file]
000083c0 20f (000083c0) _rd_cpu1
000083ee 20f (000083c0) _wr_cpu1
[Expressions]
wr_cpu1.member11 ... Address 0x000083F9@Data
wr_cpu1.member13 ... Address 0x000083FB@Data
wr_cpu1.member14 ... Address 0x000083FC@Data
wr_cpu1.member19 ... Address 0x00008401@Data
Maybe the structure wr_cpu1 at CLARAM is not alined top of data page, so C2000 compiler mistake an offset culcuration from top of structure.
This is caused the difference of architekture between C2000 CPU core and CLA core, from using DP register to access memory or not.
Is this known bug of old compiler?
And is there a way to avoid this?