Hi There,
I'm reviewing the above schematic design and I note that the current sensor output is being connected to 4 ADC pins:
Signal Name |
HSEC-180 Pin |
MCU Pin ID |
MCU Pin |
I.inv(1) |
15 |
ADC-A2 |
U2 |
I.inv(2) |
18 |
ADC-B2 |
V3 |
I.inv(3) |
28 |
ADC-D0 |
T5 |
I.inv(4) |
31 |
ADC-C2 |
R3 |
As I am looking at porting to F28377S (100 pin) I only have a limited number of ADCs and was wondering if I do need the last 2 ADC inputs? or could rewrite the code to point to the first two ADCs instead?
Thanks in advance
Robin