Other Parts Discussed in Thread: C2000WARE
Hi - The F280049C TRM references (sec's 13.1.3.2 & 13.1.3.4) the AdcSetMode function and states the function must be called at least once after device reset to ensure the correct trim is loaded into the ADC trim registers. The TRM states the function can be found in the F28004x_Adc.c file. The function is not in the file (C2000\C2000Ware_1_00_06_00\device_support\f28004x\common\source\F28004x_Adc.c). Section 13.1.12 of the TRM talks about ADC Calibration but does not mention this AdcSetMode function. Can I assume this AdcSetMode function is not required? Thx!