Tool/software: Code Composer Studio
About the two-phase interleaved boost of the TMDSHVMPPTKIT kit
I purchased the TMDSHVMPPTKIT kit and wrote the corresponding program through JTAG. The DC300V voltage was input at the input of the TMDSHVMPPTKIT kit, but the two-phase interleaved boost has no PWM waveform output, and the PWM signal of the half-bridge resonant LLC isolation stage has an output, but
The duty cycle is 10%. I don't know where the problem is. All hardware settings are fine, and Gui_Operation_mode is also set to 1, but the two-phase interleaved boost still has no PWM waveform output.