Other Parts Discussed in Thread: UNIFLASH
I want to use Uniflash and a Black Hawk XDS 200 to program a board with four F28335 (three with the same program, one different). I see from the linked thread that I cannot use one UniFlash configuration to program all four DSPs. I wonder if anyone can provide example configuration files to direct Uniflash to each DSP in turn, so I can select each DSP and program it. Ideally the example will be a .ccxml target configuration from CCS with multiple DSPs and one or more single DSP ccxml files to program each DSP in turn.