This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

F2808 : when input clock OSCCLK fails, the watch dog will not work, right?

Expert 4860 points

Replies: 4

Views: 167

Part Number: TMS320F2808

According to the datasheet, when the input clock OSCCLK fails, the watch dog counter will stop, so the watch dog reset can not be triggered, right?

请使用手机"扫一扫"x

  • That is correct, but this device has internal missing clock detection logic which will reset the device if OSCCLK fails. For more information please refer to section 3.2.2 in the TRM.

    Regards,

    Richard
  • In reply to Richard Poley:

    Correction: section 3.2.2 of this document:
    www.ti.com/.../spru712h.pdf
  • Aki,

    You are correct.  If OSCCLK fails, the WD will stop.  However, failure of OSCCLK will trigger a missing clock detect, and this will reset the device.  After coming out of reset, software can check if the OSCCLK has failed and take suitable action.  See the TRM SPRU712H, section 3.2.2.

    Regards,

    David

    -----------------------------
    David M. Alter
    Senior Member Technical Staff
    Texas Instruments Inc.

  • In reply to David M. Alter:

    David,

    Thanks!

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.