Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
I have a few questions about DRV8301-69M-KIT board, Could you help on them?
1. Is it possible to directly use the GUI to read the motor parameters, instead of having to download the program to the F28029 chip first?
2. I chose the lab2b project, is it true that if I put the .out file into the corresponding directory of the GUI after compiling, then the interface will be running my own program after the GUI is started?
3. For a CCS project (such as lab2b), is there any document to explain in details like which functions need to be called and which parameters need to be edited to start the motor and control its spin speed? I understand the speed is dependent on specific application, but after opening lab2 project, I don't know where to modify to let it combine with my actual application.
Thank you.