Dear Texas Instruments Team,
I have got a TMDSCNCD280049C control card evaluation module. During my tests, I have
programmed the GPIO37 (which is also the TDO line of JTAG) as input:
GPIO_setDirectionMode(37,GPIO_DIR_MODE_IN);
GPIO_setQualificationMode(37,GPIO_QUAL_SYNC);
GPIO_setPadConfig(37,GPIO_PIN_TYPE_STD); // disable pull up
GPIO_setPinConfig(GPIO_37_GPIO37);
This was the last time I have successfully programmed the control card. Afterwards it was not possible anymore.
Investigation has shown that ther is no answer on the TDO line from the microcontroller.
It seems that because the GPIO is programmed as an input, the JTAG cannout output test data there and as such the JTAG programming fails.
What can I do about this? I want to program the microcontroller again. Help is appreciated.
Many thanks in advance.
Best regards
Patrick