This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28069: generation of .bin file

Part Number: TMS320F28069


Tool/software: TI C/C++ Compiler

Hi,

Actually we need to generate the .bin file to upgrade the firmware.

How to generate the .bin file from CCS IDE for the TMS320F28069.

Thanks and Regards, 

Amol

  • Please see the Pre and Post Build Steps sub-chapter of the larger article on Project Management and Build.

    Thanks and regards,

    -George

  • Example_2806xGpioToggle.zipHi George,

    i followed the procedure and added the command as "${CCE_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin" "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.bin" "${CG_TOOL_ROOT}/bin/ofd2000" "${CG_TOOL_ROOT}/bin/hex2000" "${CCE_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin"

    but it is creating .bin file of more size,

    how can i reduce the size of bin file. please refer the attached bin file

  • If I see your linker map file, I suspect I will be able to tell you what happened.  Please attach it to your next post.  So the forum will accept it, please add the file extension .txt to it.

    Thanks and regards,

    -George

  • Hi George,

    Please find the below linker map file

    Thanks and Regards,

    Amol

    /*
    // TI File $Revision: /main/3 $
    // Checkin $Date: March 3, 2011 13:45:53 $
    //###########################################################################
    //
    // FILE: F28069.cmd
    //
    // TITLE: Linker Command File For F28069 Device
    //
    //###########################################################################
    // $TI Release: F2806x Support Library v2.04.00.00 $
    // $Release Date: Thu Oct 18 15:47:20 CDT 2018 $
    // $Copyright:
    // Copyright (C) 2009-2018 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without
    // modification, are permitted provided that the following conditions
    // are met:
    //
    // Redistributions of source code must retain the above copyright
    // notice, this list of conditions and the following disclaimer.
    //
    // Redistributions in binary form must reproduce the above copyright
    // notice, this list of conditions and the following disclaimer in the
    // documentation and/or other materials provided with the
    // distribution.
    //
    // Neither the name of Texas Instruments Incorporated nor the names of
    // its contributors may be used to endorse or promote products derived
    // from this software without specific prior written permission.
    //
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################
    */

    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file,
    // add the header linker command file directly to the project.
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within
    // the memory map.
    //
    // The header linker files are found in <base>\headers\cmd
    //
    // For BIOS applications add: F2806x_Headers_BIOS.cmd
    // For nonBIOS applications add: F2806x_Headers_nonBIOS.cmd
    ========================================================= */

    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper
    // locations within the memory map */

    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l F2806x_Headers_nonBIOS.cmd */

    /* Uncomment this line to include file only for BIOS applications */
    /* -l F2806x_Headers_BIOS.cmd */

    /* 2) In your project add the path to <base>\headers\cmd to the
    library search path under project->build options, linker tab,
    library search path (-i).
    /*========================================================= */

    /* Define the memory block start/length for the F2806x
    PAGE 0 will be used to organize program sections
    PAGE 1 will be used to organize data sections

    Notes:
    Memory blocks on F28069 are uniform (ie same
    physical memory) in both PAGE 0 and PAGE 1.
    That is the same memory region should not be
    defined for both PAGE 0 and PAGE 1.
    Doing so will result in corruption of program
    and/or data.

    Contiguous SARAM memory blocks can be combined
    if required to create a larger memory block.
    */

    MEMORY
    {
    PAGE 0 : /* Program Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    RAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L0 */
    RAML1 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */
    OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */

    FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH */
    FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */
    FLASHF : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */
    FLASHE : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */
    FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */
    FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */
    FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */
    CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
    BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
    CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */

    FPUTABLES : origin = 0x3FD590, length = 0x0006A0 /* FPU Tables in Boot ROM */
    IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */
    IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */
    IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */

    ROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */
    RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
    VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */

    PAGE 1 : /* Data Memory */
    /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
    /* Registers remain on PAGE1 */

    BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
    RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
    RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
    RAML2 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */
    RAML3 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3 */
    RAML4 : origin = 0x00A000, length = 0x002000 /* on-chip RAM block L4 */
    RAML5 : origin = 0x00C000, length = 0x002000 /* on-chip RAM block L5 */
    RAML6 : origin = 0x00E000, length = 0x002000 /* on-chip RAM block L6 */
    RAML7 : origin = 0x010000, length = 0x002000 /* on-chip RAM block L7 */
    RAML8 : origin = 0x012000, length = 0x002000 /* on-chip RAM block L8 */
    USB_RAM : origin = 0x040000, length = 0x000800 /* USB RAM */
    FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */
    }

    /* Allocate sections to memory blocks.
    Note:
    codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
    execution when booting to flash
    ramfuncs user defined section to store functions that will be copied from Flash into RAM
    */


    SECTIONS
    {

    /* Allocate program areas: */
    .cinit : > FLASHH, PAGE = 0
    .pinit : > FLASHH, PAGE = 0
    .text : > FLASHH, PAGE = 0
    codestart : > BEGIN, PAGE = 0
    ramfuncs : LOAD = FLASHD,
    RUN = RAML0,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    LOAD_SIZE(_RamfuncsLoadSize),
    PAGE = 0

    csmpasswds : > CSM_PWL_P0, PAGE = 0
    csm_rsvd : > CSM_RSVD, PAGE = 0

    /* Allocate uninitialized data sections: */
    .stack : > RAMM0, PAGE = 1
    .ebss : > RAML4, PAGE = 1
    .esysmem : > RAML2, PAGE = 1
    .cio : > RAML5, PAGE = 1

    /* Initialized sections to go in Flash */
    /* For SDFlash to program these, they must be allocated to page 0 */
    .econst : > FLASHH, PAGE = 0
    .switch : > FLASHH, PAGE = 0

    /* Allocate IQ math areas: */
    IQmath : > FLASHH, PAGE = 0 /* Math Code */
    IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD

    /* Allocate FPU math areas: */
    FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD

    DMARAML5 : > RAML5, PAGE = 1
    DMARAML6 : > RAML6, PAGE = 1
    DMARAML7 : > RAML7, PAGE = 1
    DMARAML8 : > RAML8, PAGE = 1

    /* Uncomment the section below if calling the IQNexp() or IQexp()
    functions from the IQMath.lib library in order to utilize the
    relevant IQ Math table in Boot ROM (This saves space and Boot ROM
    is 1 wait-state). If this section is not uncommented, IQmathTables2
    will be loaded into other memory (SARAM, Flash, etc.) and will take
    up space, but 0 wait-state is possible.
    */
    /*
    IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
    {

    IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

    }
    */
    /* Uncomment the section below if calling the IQNasin() or IQasin()
    functions from the IQMath.lib library in order to utilize the
    relevant IQ Math table in Boot ROM (This saves space and Boot ROM
    is 1 wait-state). If this section is not uncommented, IQmathTables2
    will be loaded into other memory (SARAM, Flash, etc.) and will take
    up space, but 0 wait-state is possible.
    */
    /*
    IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
    {

    IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)

    }
    */

    /* .reset is a standard section used by the compiler. It contains the */
    /* the address of the start of _c_int00 for C Code. /*
    /* When using the boot ROM this section and the CPU vector */
    /* table is not needed. Thus the default type is set here to */
    /* DSECT */
    .reset : > RESET, PAGE = 0, TYPE = DSECT
    vectors : > VECTORS, PAGE = 0, TYPE = DSECT

    }

    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */

  • Unfortunately, you sent the linker command file, which is a different file than the linker map file.  The linker command file is an important input to the link.  The linker map file is an output from the link.  It is a text file which shows, among other things, how sections are formed and allocated to memory.  In a CCS project, the linker map file has the same name as the project, with the extension .map.  It is found in the Debug directory, or whatever is the name of the current build configuration.

    Please locate the linker map file, add the file extension .txt, and attach it to your next post.  Please do not copy-n-paste the contents of the file directly inside the post.

    Thanks and regards,

    -George

  • Please submit the linker map file as described in the previous post.

    Thanks and regards,

    -George

  • Hi George,

    Thanks for the input ,

    As i changed my linker cmd file with conjugative memory locations , it resolved my issue and i verified with linker map file.

    Thanks and Regards,

    Amol