Other Parts Discussed in Thread: POWERSUITE
Hi There,
I'm stepping through TIDUAY6D (Revised May 2019), specifically step 3.1.2.3.3 Step 6: observing invliInst as I raise the DC bus and I do not see it regulating as the bus voltage goes above 50VDC.
As per the note following step 8, i did complete Build 1 steps and verify the voltage and current sensing parameters were correct; I then went back to the compensation designer section to try and review the gain at DC settings but I was not able to follow how this is done.
Can you please advise me on how to alter the compensation designer such that I can complete Build 2 of the user guide?
Note: I had an issue with selecting "COMPI" in the Control Loop Design section initially, however after pasting in an empty ".cookie" file into the folder and restarting CCS I was then able to select COMPI.
Thanks in advance
Robin
CCS - V9.01
Digital PowerSDK - 1.03
PowerSuite 2.04